Hi,
Up until kernel 3.14.52_1.1.1_ga, the TapeOut (TO) 1.0 of the i.MX6Q was supported fine.
But since the 4.1.15_1.2.0_ga, and earlier 4.1.15 tags too, the i.MX6Q TO1.0 doesn't run Linux properly. It seems that the clocking is wrong and the board becomes very slow.
The Release Notes doesn't mention any minimal processor revision so it is assumed even the TO1.0 should be supported.
Please advise.
Regards,
Gary
已解决! 转到解答。
Hi Gary
it was dropped since L3.0.35_4.1.1
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Gary
it was dropped since L3.0.35_4.1.1
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------