Issue flashing i.MX8MM SD card with UUU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue flashing i.MX8MM SD card with UUU

4,261 Views
michaelworster
Contributor IV

I've been trying to flash the SD card on my i.MX8MM and been having some issues. I've looked into the documentation but it doesn't quite clear up my confusion.

For UUU I've downloaded the latest 1.4.127: https://github.com/NXPmicro/mfgtools/releases/tag/uuu_1.4.127

And I've also downloaded the latest pre-build Linux binaries L5.10.9_1.0.0_MX8MM: https://www.nxp.com/webapp/Download?colCode=L5.10.9_1.0.0_MX8MM&appType=license

I used UUU to flash this 5.10 Linux release into my eMMC via:

uuu.exe uuu.auto

 

That flashed and booted just fine. I then tried to flash this to the SD card simply by updating the uuu.auto file as follows:

# SD Programming:
FB: ucmd setenv fastboot_dev mmc
FB: ucmd setenv mmcdev ${sd_dev}
FB: ucmd mmc dev ${sd_dev}
FB: flash -raw2sparse all imx-image-multimedia-imx8mmevk.wic
FB: flash bootloader imx-boot-imx8mmevk-sd.bin-flash_evk
FB: ucmd if env exists sd_ack; then ; else setenv sd_ack 0; fi;
FB: ucmd mmc partconf ${sd_dev} ${sd_ack} 1 0
FB: done

# Emmc programming:
#FB: ucmd setenv fastboot_dev mmc
#FB: ucmd setenv mmcdev ${emmc_dev}
#FB: ucmd mmc dev ${emmc_dev}
#FB: flash -raw2sparse all imx-image-multimedia-imx8mmevk.wic
#FB: flash bootloader imx-boot-imx8mmevk-sd.bin-flash_evk
#FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;
#FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0
#FB: done

 

This failed at the following step:

uuu.exe uuu.auto
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.127-0-g08c58c9

Success 0    Failure 1


2:2      7/ 8 [                                      ] FB: ucmd mmc partconf ${sd_dev} ${sd_ack} 1 0

 

Which makes me think I can't simply swap one for the other. So my question is, how can I use uuu to flash the v5.10 pre-released Linux binaries to the SD card on the i.MX8MM EVK?

Labels (1)
0 Kudos
Reply
4 Replies

4,246 Views
BiyongSUN
NXP Employee
NXP Employee

just one command line using uuu build-in command

uuu -b sd_all imx-boot-imx8mmevk-sd.bin-flash_evk imx-image-multimedia-imx8mmevk.wic

suggest to read the uuu manual or type uuu without parameter to show the help

0 Kudos
Reply

4,241 Views
michaelworster
Contributor IV

Thanks for the input. The documentation and the `uuu` output both mention the sdcard if flashed via a `.sdcard` file:

   sd_all  burn whole image to sd card
                arg0: _flash.bin
                arg1: _rootfs.sdcard

 

Clearly in this case it was a `.wic` file instead. Is that mentioned somewhere that I missed?

 

Second question: while the built in command works, can the uuu.auto file be used as well for SD card flashing?

0 Kudos
Reply

4,229 Views
BiyongSUN
NXP Employee
NXP Employee

It no problem to use script. 

What you need is the common basic knowledge. 

Because from the "FB: ucmd mmc partconf ${sd_dev} ${sd_ack} 1 0", know about you have no any knowledge about emmc and sd card as you don't know about the wic.

Here is the script to flash the sdcard. uuu uuu.sd.auto to use it.


uuu.sd.auto

uuu_version 1.2.39

# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ
SDP: boot -f imx-boot-imx8mmevk-sd.bin-flash_evk

# This command will be run when ROM support stream mode
# i.MX8QXP, i.MX8QM
SDPS: boot -f imx-boot-imx8mmevk-sd.bin-flash_evk

# These commands will be run when use SPL and will be skipped if no spl
# SDPU will be deprecated. please use SDPV instead of SDPU
# {
SDPU: delay 1000
SDPU: write -f imx-boot-imx8mmevk-sd.bin-flash_evk -offset 0x57c00
SDPU: jump
# }

# These commands will be run when use SPL and will be skipped if no spl
# if (SPL support SDPV)
# {
SDPV: delay 1000
SDPV: write -f imx-boot-imx8mmevk-sd.bin-flash_evk -skipspl
SDPV: jump
# }

FB: ucmd setenv fastboot_dev mmc
FB: ucmd setenv mmcdev ${emmc_sd}
FB: ucmd mmc dev ${emmc_sd}
FB: flash -raw2sparse all imx-image-multimedia-imx8mmevk.wic
FB: done

 

Untitled.png

0 Kudos
Reply

4,232 Views
BiyongSUN
NXP Employee
NXP Employee

to know what is wic, you should have the yocto knowledge. 

and wic is same as .sdcard.  

 

 

0 Kudos
Reply