Is there anyway to connect 2 Gbyte of LPDDR2 to an i.MX53 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there anyway to connect 2 Gbyte of LPDDR2 to an i.MX53 ?

981件の閲覧回数
pierreschirrer
Contributor II

Hello community,

I designed a board with an i.MX53 and 1Gbyte of LPDDR2 using Micron memory, MT42L256M32D2 (16Meg x 32 x 8 banks x 2 die). Now I was asked to increase the memory to 2Gbytes. Unfortunately, Micron has not issued the MT42L512M32D4 (32 Meg x 16 x 8 banks x 4 die)...

Does anybody know how to connect several LPDDR2 chips to the SDRAM controller of the i.MX53 (there is only one SDRAM channel with only 2 chip selects on the i.MX53) ?

Any help would be appreciated,

Thanks.

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

841件の閲覧回数
Yongxin
NXP Employee
NXP Employee

Hi Pierre Schirrer,

Due to the configuration addressing of MT42L256M32D2, it is impossible to connect two MT42L256M32D2 in i.MX53.

The iMX53 is capable of addressing 2GB on CS0. Or if use both CS0 and 1, it can address 1GB on each one. It is recommended to use other LPDDR2 chip for the design.

Best Regards,

Yongxin

841件の閲覧回数
pierreschirrer
Contributor II

Thank you Yongxin Huang,

It is as I feared.

0 件の賞賛
返信