SIM CNTL register bits in the document (i.MX 6UltraLite Applications Processor Reference Manual Document Number: IMX6ULRM Rev. 0, 08/2015)
SIM CNTL register bits in the code( BSP 3.14.38_6ul , <linux_dir>driver/mxc/SIM/mxc_sim.c), I didn't change anything.
we can see, the first bit to the third correspond to the document, others do not.
Is the content of IMX6ULRM about EMV wrong?
已解决! 转到解答。
Hello Huang,
The reference Manual it is correct, the Linux driver that you find it is not for the i.MX6UL it is from the i.MX25 which has the SIM module and the SIM CNTL register it is exactly the way it is described, in fact if you see in the i.MX6UL the register name is EMVSIMx_CTRL . I apologize for this inconvenience.
Have a nice day!
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------