Is the content of IMX6ULRM about EMV wrong?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is the content of IMX6ULRM about EMV wrong?

ソリューションへジャンプ
1,909件の閲覧回数
dmaker
Contributor II

SIM CNTL register bits in the document  (i.MX 6UltraLite Applications Processor Reference Manual   Document Number: IMX6ULRM Rev. 0, 08/2015)

文档.png

SIM CNTL register bits in the code( BSP 3.14.38_6ul ,  <linux_dir>driver/mxc/SIM/mxc_sim.c), I didn't change anything.

源码.png

we can see,  the first bit to the third  correspond to the document, others do not.

Is the content  of  IMX6ULRM about  EMV  wrong?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,469件の閲覧回数
dmaker
Contributor II

I get it,the correct document about mxc_sim.c is in 45 chapters,not in 22 chapters.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,469件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Huang,

The reference Manual it is correct,  the  Linux driver that you find it is not for the i.MX6UL it is from the i.MX25 which has the SIM module and the SIM CNTL register it is exactly the way it is described, in fact if you see in the i.MX6UL the register name is  EMVSIMx_CTRL .  I apologize for this inconvenience.

Have a nice day!


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,469件の閲覧回数
dmaker
Contributor II

But i found the code from the BSP which had already source MACHINE=imx6ulevk.  Now, I do know how to get the linux driver for the i.mx6ul.

0 件の賞賛
返信
1,469件の閲覧回数
dmaker
Contributor II

And I print out all default values of the registers from 0x021B4000.(0xF43B4000 map to 0x021B4000)

pastedImage_0.png

and the default values in the document

pastedImage_1.png

there is a very big difference.

0 件の賞賛
返信
1,470件の閲覧回数
dmaker
Contributor II

I get it,the correct document about mxc_sim.c is in 45 chapters,not in 22 chapters.

0 件の賞賛
返信