Is it possible to connect a MIPI CSI-1 device to i.MX8MMini and SN65LVDS315 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to connect a MIPI CSI-1 device to i.MX8MMini and SN65LVDS315 ?

Jump to solution
1,269 Views
ko-hey
Senior Contributor II

Hi all,

 

Is SN65LVDS315 (MIPI CSI-1) compatible with our i.MX8MMini MIPI CSI-2 interface ?

CSI-2 extends CSI-1 with multiple lanes, but both standards use the same D-PHY layer.

 

According to the following thread, it can't connect with i.MX6 and SN65LVDS315 due to the difference of standard.

https://community.nxp.com/docs/DOC-96385

 

We guess that it's same as i.MX8MMini. Am I correct ?

 

Ko-hey

 

0 Kudos
Reply
1 Solution
1,213 Views
mrudangshelat1
Senior Contributor II

HI Ko-Hey,

Yes, the CSI-2 interface is not compatible with CSI-1 devices and cannot use SN65LVDS315 for CSI-2 Interface.

Regards,

Mrudang

View solution in original post

1 Reply
1,214 Views
mrudangshelat1
Senior Contributor II

HI Ko-Hey,

Yes, the CSI-2 interface is not compatible with CSI-1 devices and cannot use SN65LVDS315 for CSI-2 Interface.

Regards,

Mrudang