Imx6ul use 1280*800 display, how many frames can be displayed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx6ul use 1280*800 display, how many frames can be displayed

1,049件の閲覧回数
liangmu
Contributor I

Dear ,

I use the imx6ul evk baseline, and the screen resolution is set to 1280*800, and how much is the frame rate set at this time? Will the shadow be displayed?

Thinks

0 件の賞賛
返信
3 返答(返信)

901件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi liang

as i.MX6UL has not VPU, all codec operations are performed in software

and framerate depends mainly on processor load (use case). In nxp bsps

software codec performance is described in  Table 30. Video codec specification for

hardware without VPU acceleration attached Release Notes, for resolution 1280*800

it may be recalculated accordingly.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

901件の閲覧回数
liangmu
Contributor I

Dear,

"Nxp bsps software codec performance is described in  Table 30",Which document?

0 件の賞賛
返信

901件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

document in attachment previous answer (in red).

pastedImage_3.jpg

0 件の賞賛
返信