Dear ,
I use the imx6ul evk baseline, and the screen resolution is set to 1280*800, and how much is the frame rate set at this time? Will the shadow be displayed?
Thinks
Hi liang
as i.MX6UL has not VPU, all codec operations are performed in software
and framerate depends mainly on processor load (use case). In nxp bsps
software codec performance is described in Table 30. Video codec specification for
hardware without VPU acceleration attached Release Notes, for resolution 1280*800
it may be recalculated accordingly.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear,
"Nxp bsps software codec performance is described in Table 30",Which document?
document in attachment previous answer (in red).