Imx6dl with 16bit DDR3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Imx6dl with 16bit DDR3

793 次查看
adrian_dusinski
Contributor II

adrian_dusinski_0-1653928871293.png

Regarding the image above Imx6dl support only 32 and 64 bit DDR3 but is it completely impossible to use 16 bit DDR?

Regards,

Adrian

 

标签 (1)
0 项奖励
回复
2 回复数

770 次查看
adrian_dusinski
Contributor II

Thanks for reponse.

0 项奖励
回复

785 次查看
joanxie
NXP TechSupport
NXP TechSupport

refer to the data sheet:

External memory interfaces: The i.MX 6Solo/6DualLite processors support latest, high volume,
cost effective handheld DRAM, NOR, and NAND Flash memory standards.
— 16/32-bit LP-DDR2-800, 16/32-bit DDR3-800 and DDR3L-800 in i.MX 6Solo; 16/32/64-bit
LP-DDR2-800, 16/32/64-bit DDR3-800 and DDR3L-800, supporting DDR interleaving mode
for 2x32 LPDDR2-800 in i.MX 6DualLite

 

0 项奖励
回复