Imx6dl Android P9.0.0_2.2.0 ethernet(usb ethernet) link is up but ping fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx6dl Android P9.0.0_2.2.0 ethernet(usb ethernet) link is up but ping fail

1,706件の閲覧回数
chpub70
Contributor II

Hi NXP,

I am using a custom imx6dl board with android_p9.0.0_2.2.0-ga. From the command line, I did ifconfig eth0 up 192.168.30.240 and I did ip link and I can see the link is up.

130|sabresd_6dq:/ # ip link
1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue state UNKNOWN mode DEFAULT group default qlen 1000
link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
2: ip_vti0@NONE: <NOARP> mtu 1480 qdisc noop state DOWN mode DEFAULT group default qlen 1000
link/ipip 0.0.0.0 brd 0.0.0.0
3: ip6_vti0@NONE: <NOARP> mtu 1500 qdisc noop state DOWN mode DEFAULT group default qlen 1000
link/tunnel6 :: brd ::
4: sit0@NONE: <NOARP> mtu 1480 qdisc noop state DOWN mode DEFAULT group default qlen 1000
link/sit 0.0.0.0 brd 0.0.0.0
5: ip6tnl0@NONE: <NOARP> mtu 1452 qdisc noop state DOWN mode DEFAULT group default qlen 1000
link/tunnel6 :: brd ::
6: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc pfifo_fast state UP mode DEFAULT group default qlen 1000
link/ether 00:de:fa:87:6e:d7 brd ff:ff:ff:ff:ff:ff

However when I did ifconfig eth0, I see all received packet is dropped.

sabresd_6dq:/ # ifconfig eth0
eth0 Link encap:Ethernet HWaddr 00:de:fa:87:6e:d7 Driver smsc95xx
inet addr:192.168.30.240 Bcast:192.168.30.255 Mask:255.255.255.0
inet6 addr: fe80::2de:faff:fe87:6ed7/64 Scope: Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:13270 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 TX bytes:0

Please advise. 

Thank You in advance.

Regards,

Pun

0 件の賞賛
返信
5 返答(返信)

1,659件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

when the board boot up, could you ping successfully?

0 件の賞賛
返信

1,659件の閲覧回数
chpub70
Contributor II

Hi Joan,

No, I cannot ping successfully.

0 件の賞賛
返信

1,658件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

pls share your log file with me

0 件の賞賛
返信

1,659件の閲覧回数
chpub70
Contributor II

Hi Joan,

Attach is the log for dmesg and logcat.

0 件の賞賛
返信

1,542件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

what PHY do you use? the same as nxp board? or porting your own PHY? and could you reproduce this on nxp board?

0 件の賞賛
返信