INNOSTICK6 NXP i.MX6ULL based Computer Board in a small form factor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

INNOSTICK6 NXP i.MX6ULL based Computer Board in a small form factor

703 Views
weidongzhou
Contributor I

INNOSTICK6-2_560.jpg

Based on NXP/Freescale's i.MX6ULL ARM Cortex-A7 processor with up to 900MHz CPU Clock, the INNOSTICK 6 is a portable and easy-to-use computer which integrated with on board DDR3 memory and eMMC storage in a tiny form factor(80mmx42mm). The INNOSTICK 6 provides a variety of interfaces and connectivity options - all packaged at an optimized power, size and cost. The INNOSTICK 6 highly integrated connectivity includes Wi-Fi, Bluetooth/BLE, USB Host and OTG, Camera, LCD display with touch panel and serial interfaces.

ikbd3_560.jpg

Labels (2)
0 Kudos
Reply
0 Replies