IMX8QXP uses Q10.0.0_2.2.0_AUTO_SOURCE and requires NVP6324 driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8QXP uses Q10.0.0_2.2.0_AUTO_SOURCE and requires NVP6324 driver

691 Views
relax-wu
Contributor IV

The current project uses NVP6324, is there a corresponding driver patch?

0 Kudos
Reply
2 Replies

680 Views
igorpadykov
NXP Employee
NXP Employee

Hi relax-wu

 

please refer to below patch:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Nvp6324-driver-for-imx8qm/ta-p/1114616

 

Best regards
igor

0 Kudos
Reply

670 Views
relax-wu
Contributor IV

Hi

If the driver migration is successful and the hardware path is normal, is it tested through the camera application that comes with the system?

0 Kudos
Reply