IMX8QXP,How can I control the gpio.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8QXP,How can I control the gpio.

ソリューションへジャンプ
3,989件の閲覧回数
xinchuan
Contributor III

Hello,

IMX8QXP MEK Board, android_O8.1.0_1.1.0_AUTO-EAR.

I can control SC_P_MIPI_CSI0_GPIO0_00_MIPI_CSI0_GPIO0_IO00 using the codes below.

now I need to control SC_P_MIPI_DSI0_GPIO0_00_MIPI_DSI0_GPIO0_IO00,

How can I get the boldfaced words's information ? please.

Thanks.

gpio0_mipi_csi0: gpio@58222000 {
compatible = "fsl,imx8qm-gpio", "fsl,imx35-gpio";
reg = <0x0 0x58222000 0x0 0x1000>;
interrupts = <0 IRQ_TYPE_LEVEL_HIGH>;
interrupt-parent = <&irqsteer_csi>;
gpio-controller;
#gpio-cells = <2>;
interrupt-controller;
#interrupt-cells = <2>;
power-domains = <&pd_mipi_csi>;
clocks = <&clk IMX8QXP_CSI0_IPG_CLK_S>;
clock-names = "ipg";
};

pinctrl_mipi_csi0_gpio: mipicsi0gpiogrp{
fsl,pins = <
SC_P_MIPI_CSI0_GPIO0_00_MIPI_CSI0_GPIO0_IO00 0x00000021
SC_P_MIPI_CSI0_GPIO0_01_MIPI_CSI0_GPIO0_IO01 0x00000021
>;
};


&gpio0_mipi_csi0 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_mipi_csi0_gpio>;
};

pwn-gpios = <&gpio0_mipi_csi0 0 GPIO_ACTIVE_HIGH>;




max9286_data->pwn_gpio = of_get_named_gpio(dev->of_node, "pwn-gpios", 0);
if (!gpio_is_valid(max9286_data->pwn_gpio)) {
dev_err(dev, "no sensor pwdn pin available\n");
return -ENODEV;
}
retval = devm_gpio_request_one(dev, max9286_data->pwn_gpio, GPIOF_OUT_INIT_LOW,
"max9286_pwd");
pr_err("XXCC set r1237--\n");
while(1)
{
gpio_set_value(max9286_data->pwn_gpio, 1);
msleep(2000);
gpio_set_value(max9286_data->pwn_gpio, 0);
msleep(2000);
}

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,100件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi,

please take a look here GPIO configuration 

If you are interested in developing a kernel module to handle GPIOs I can share a snippet, just let me know because I have to find it.


Regards,
Carlos
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,101件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi,

please take a look here GPIO configuration 

If you are interested in developing a kernel module to handle GPIOs I can share a snippet, just let me know because I have to find it.


Regards,
Carlos
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,100件の閲覧回数
xinchuan
Contributor III

Hi Carlos,

      Thanks for your reply,and it's helpful.

Thanks & Regards

Chuan

0 件の賞賛
返信