IMX8QM-MEK M.2 Slot compatibility

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8QM-MEK M.2 Slot compatibility

1,817件の閲覧回数
jishin42
Contributor III

Hi,

 

On the  iMX 8 QuadMax MEK (MCIMX8QM-CPU), there is a M.2 slot (key E) to connect Wifi/bluetooth modules.

I would like to use this connector to link the iMX8 to another CPU via PCIe.

Is there enough space on the left of the M.2 slot to insert an A+E keyed M.2 board ?

For instance : M.2-A+E-to-Mini-PCI-Adapter-Cable

M.2 (NGFF) Key A/E/A+E to Mini PCI-E

Thank you,

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,655件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jishin42,

Due to its placement on the board and the form of the module you wish to use I would think it should fit but I cannot be certain. You can see the front and back of the board on the Getting Started on the link below:

Get Started with the i.MX 8QuadMax MEK | NXP 

I hope this helps!

Regards,

0 件の賞賛
返信