IMX8Mplus ISP for RGB to YUV and Bayer in hardware ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8Mplus ISP for RGB to YUV and Bayer in hardware ?

1,327件の閲覧回数
glen1
Contributor I

We are looking at replacing our TI DaVinci platform with this new device.
We have DUAL vision sensor inputs.

Can the ISP on the IMX8M plus device perform color space RGB >> YUV conversion (required for input for the H264 encoder) ? (in hardware, not software) 

Can it also perform Bayer dematrixing ? (in hardware, not software) 
Required rate is 110 Mpx/sec.


another way to ask, can the device use RGB raw sensors or must use YUV image sensors ?


There is no tech manual for the processor yet, hence the question..

with thanks, Glen English.

0 件の賞賛
返信
1 返信

1,068件の閲覧回数
khang_letruong
Senior Contributor III

Hi @glen1 ,

In the RM of iMX 8M Plus, the input formats of ISP are below :

ISP_INPUTs.png

Regards,
Khang.

0 件の賞賛
返信