Hi,
Customer SKF: is asking for Altium format design files for 8Mplus-EVK Base Board and CPU Module.
As alternative the .ALG files of the two boards which might in case be imported into Altium Tool.
thanks and best regards
Massimo Incerti
已解决! 转到解答。
@zmlopez
Hello,
We do not provide design files for Altium.
Customers can try the following approach:
Regards,
Yuri.
Dear Yuri,
I´m also looking for tha altium files for the bb46370 and for the pvk46881 boards.
I have the .alg files converted from the .brd original files, but i´m missing the footprints.
Can you help me?
I need to design a custom base board with only a few peripherals with strong space constraints (thinking on 100K boards and the lack of the complete altium project is delaying the project.
Thanks in advance.
marcos.-
Hi, Yuri.
Can you please send a reference on where we can load schematic/reference files - we are planning to start working on SOM based on i.MX8M.
The board we have and ideally for which we need design files is 8MPLUSPLD4-EVK
Thanks in advance.
Sergei Danielian
@sergeidanielian
Hello,
Please use the following resources:
https://www.nxp.com/webapp/Download?colCode=8MPLUSLPD4-PWR-DESIGN-FILES
https://www.nxp.com/downloads/en/schematics/8MPLUS-BB.zip
https://www.nxp.com/downloads/en/schematics/8MPLUSLPD4-CPU.zip
Regards,
Yuri.