We are facing a problem in our board which was developed based on the IMX8MP board. We got a patch from NXP to modify the BSP for 2GB board and it is working for W21H2-1-3-0 BSP. Then we tried this patch in Windows 10 IoT BSP W21H2-1-4-1 but the board is not booting now with this patch. Is there any new patch?
Hi @Bio_TICFSL , Is there any update?
Hi @Bio_TICFSL , Is there any update on this?
Hello,
Yes it works with linux BSP it does not with windows you need a new version of windows to support wifi.
Regards
Hi @Bio_TICFSL , We got patch from NXP for Windows 10 IoT W21H2-1-3-0 BSP only and it is working. We have tried this patch in Windows 10 IoT BSP W21H2-1-4-1 but the board is not booting.
IMX8MP RAM ISSUE - NXP Community - This is previously we have addressed.