Hello,
In the user manual under paragraph 13.9.1.2 there is a block diagram (Figure 13-104) which shows TX and RX signals which can be used for i2S. My question is:
Kind Regards,
Den
解決済! 解決策の投稿を見る。
Hi Den
>Would it be possible to drive both if I connect them in the following manner..
yes such connection is possible
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Den
>Would it be possible to drive both if I connect them in the following manner..
yes such connection is possible
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------