IMX8-QXP + SXF1800: v2xse-example-app issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8-QXP + SXF1800: v2xse-example-app issue

1,135 次查看
PBR
Contributor IV

Hello,

With a IMX8-QXP, I try to access SXF1800 with v2xse-example-app.

First I reset SXF1800 (command 04)
Secondly I try to activate it (command 01).
I select EU applet.
So the IMX8-QXP sends an I-block with 19 bytes to the SXF1800 (see v2xAppletSelect() in v2xSe.c file).
But the SXF1800 answers "A5 92 00 92" bytes meaning "other error".

How could I have more information about this error?

 

If I do:
04 - reset
03 - connect
It is working so the SPI access is working.

So how do I activate SXF1800?

Do I miss a step?

Thank you for your help.

 

0 项奖励
回复
4 回复数

1,084 次查看
PBR
Contributor IV

Please is there anybody who could provide me SXF1800 documentation how to use it?

0 项奖励
回复

1,128 次查看
PBR
Contributor IV

Any help?

0 项奖励
回复

1,114 次查看
PBR
Contributor IV

Please some help...

0 项奖励
回复

1,098 次查看
PBR
Contributor IV

Nobody can help me?

0 项奖励
回复