IMX7D ADC offset issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX7D ADC offset issue

1,117件の閲覧回数
frankyhsu
Contributor III

Hi

We measure the ADC input voltage and read the ADC value in kernel. The input voltage is changed by thermal NTC. We found we will have a voltage difference about 0.032~0.048V between ADC read and voltage measurement. How to decrease difference between them? The drift seems to be too much.

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

886件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Franky

one can check stability and noise of adc power : VDDA_ADCx_1P8, VDDA_1P0_CAP.

If voltage difference is constant, it may be removed by software.

Also may be recommended to check ground lines for thermal NTC and adc,

they should be connected in one point. Note, this is applicable to performing measurements too.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

886件の閲覧回数
frankyhsu
Contributor III

Which ground is meant for ADC ground line to connect to NTC ground?

0 件の賞賛
返信

886件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

could you short NTC to check if drift will remain

Best regards
igor

0 件の賞賛
返信

886件の閲覧回数
frankyhsu
Contributor III

We have the connection as below since we hope to have a clean power so we use 1.5V LDO from PMIC. Will the different power source affect the power accuracy?

pastedImage_1.png

0 件の賞賛
返信

886件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

>Will the different power source affect the power accuracy?

no

Best regards
igor

0 件の賞賛
返信