Hi why my sdcard image for IMX6ULVK using kernel version3.14.38-6UL_ga is showing 880 MB.
-rwxrwxrwx 1 linux linux 868220928 Jul 5 13:18 fsl-image-gui-imx6ulevk-20160705113519.rootfs.ext3
-rwxrwxrwx 1 linux linux 41077 Jul 5 13:17 fsl-image-gui-imx6ulevk-20160705113519.rootfs.manifest
-rwxrwxrwx 1 linux linux 884998144 Jul 5 13:20 fsl-image-gui-imx6ulevk-20160705113519.rootfs.sdcard
-rwxrwxrwx 1 linux linux 161179609 Jul 5 13:18 fsl-image-gui-imx6ulevk-20160705113519.rootfs.tar.bz2
lrwxrwxrwx 1 linux linux 50 Jul 5 13:20 fsl-image-gui-imx6ulevk.ext3 -> fsl-image-gui-imx6ulevk-20160705113519.rootfs.ext3
lrwxrwxrwx 1 linux linux 54 Jul 5 13:20 fsl-image-gui-imx6ulevk.manifest -> fsl-image-gui-imx6ulevk-20160705113519.rootfs.manifest
lrwxrwxrwx 1 linux linux 52 Jul 5 13:20 fsl-image-gui-imx6ulevk.sdcard -> fsl-image-gui-imx6ulevk-20160705113519.rootfs.sdcard
lrwxrwxrwx 1 linux linux 53 Jul 5 13:20 fsl-image-gui-imx6ulevk.tar.bz2 -> fsl-image-gui-imx6ulevk-20160705113519.rootfs.tar.bz2
-rwxrwxrwx 2 linux linux 1201077 Jul 5 11:48 modules--3.14.38-r0-imx6ulevk-20160705113519.tgz
lrwxrwxrwx 1 linux linux 48 Jul 5 11:48 modules-imx6ulevk.tgz -> modules--3.14.38-r0-imx6ulevk-20160705113519.tgz
-rwxrwxrwx 2 linux linux 294 Jul 5 13:12 README_-_DO_NOT_DELETE_FILES_IN_THIS_DIRECTORY.txt
lrwxrwxrwx 1 linux linux 24 Jul 5 13:00 u-boot.imx -> u-boot-sd-2015.04-r0.imx
lrwxrwxrwx 1 linux linux 24 Jul 5 13:00 u-boot-imx6ulevk.imx -> u-boot-sd-2015.04-r0.imx
-rwxrwxrwx 2 linux linux 359424 Jul 5 13:00 u-boot-sd-2015.04-r0.imx
lrwxrwxrwx 1 linux linux 47 Jul 5 11:48 zImage -> zImage--3.14.38-r0-imx6ulevk-20160705113519.bin
-rwxrwxrwx 2 linux linux 34342 Jul 5 11:48 zImage--3.14.38-r0-imx6ul-14x14-evk-20160705113519.dtb
-rwxrwxrwx 2 linux linux 34338 Jul 5 11:48 zImage--3.14.38-r0-imx6ul-14x14-evk-csi-20160705113519.dtb
-rwxrwxrwx 2 linux linux 6011120 Jul 5 11:48 zImage--3.14.38-r0-imx6ulevk-20160705113519.bin
lrwxrwxrwx 1 linux linux 58 Jul 5 11:48 zImage-imx6ul-14x14-evk-csi.dtb -> zImage--3.14.38-r0-imx6ul-14x14-evk-csi-20160705113519.dtb
lrwxrwxrwx 1 linux linux 54 Jul 5 11:48 zImage-imx6ul-14x14-evk.dtb -> zImage--3.14.38-r0-imx6ul-14x14-evk-20160705113519.dtb
lrwxrwxrwx 1 linux linux 47 Jul 5 11:48 zImage-imx6ulevk.bin -> zImage--3.14.38-r0-imx6ulevk-20160705113519.bin
hi jimmychan after going through the error which I got ERROR: Task 71 (/home/plum_project/sources/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.14.28.bb, do_install) failed with exit code '1' after bitbaking core-image-minimal it is actually bitbaking the 3.14.28 kernel version and it didnt have support for imx6ulevk.
So, after going through all the bb files i thought of using poky-tiny distro, sources/poky/meta-yocto/conf/distro/poky-tiny.bb
I changed some of the configuration
PREFERRED_PROVIDER_virtual/kernel = "linux-imx"
PREFERRED_VERSION_linux-imx = "3.14.38"
after that I ran bitbake core-image-minimal it is successful and generated the images.
One last check point is, it didnt generate sdcard images instead it genertaed core-image-minimal-imx6ulevk-20160708092743.rootfs.cpio.gz
These steps maybe useful for the people who use 3.14.38 for imx6ulevk for core-image-minimal
please try to create a new build folder for the new build.
DISTRO=<distro name> MACHINE=<machine name> source fsl-setup-release.sh -b <build dir>
Hi jimmychan i tried bitbake core-image-minimal
but i got below error
DEPMOD 3.14.28-1.0.0_ga+g91cf351
| NOTE: make -j 2 imx6ul-14x14-evk.dtb
| make[3]: *** No rule to make target `arch/arm/boot/dts/imx6ul-14x14-evk.dtb'. Stop.
| make[2]: *** [imx6ul-14x14-evk.dtb] Error 2
| make[1]: *** [sub-make] Error 2
| make: *** [all] Error 2
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_install (log file is located at /home/plum_project/Image_Minimal/tmp/work/imx6ulevk-poky-linux-gnueabi/linux-imx/3.14.28-r0/temp/log.do_install.7376)
ERROR: Task 71 (/home/plum_project/sources/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.14.28.bb, do_install) failed with exit code '1'
I am using the below repo
repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.38-6UL_ga
your rootfs need 868MB
jimmychan how can i reduce the rootfs size......my zImage is nly 6MB...for my project we planned to use nly 256 MB size of sdcard
It depends what you build and install in the rootfs. you can try to build the core-image-minimal. You will get the small size of rootfs.