IMX6SOLOX PCIE CLK CONNECTION

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6SOLOX PCIE CLK CONNECTION

662 Views
1773750986
Contributor I

Hello,smart  NXP Technical staff, now  i  use  ASM1061 converting  PCIE to  sata,i came  across a question,when  i interface the imx6solox  PCIE_CLKP and PCIE_CLKN  to  ASM1061, is  there still a need  to  add  Series capacitor C295 and C296, and  termination  resistors R68,R69,R70,R71?Waiting for  your  reply.

PCIE.png

ASM1061 PCEI CLK  PCI Express Differential Reference Clock Input Ranges

CLK.png

Labels (1)
0 Kudos
Reply
1 Reply

600 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhang

for i.MX6SX PCIe connections recommended to follow i.MX6SX Sabre reference schematic

SPF-27962 p.16

Schematics (1)
IMX6SOLOX-SABRESDB-DESIGNFILES
i.MX 6SoloX SABRE Development Board|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply