IMX6Q capture 1280*1024 pixels,114 MHz pixel clock grey image data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q capture 1280*1024 pixels,114 MHz pixel clock grey image data

802 Views
zhangyanan
Contributor I

Hi, I am writing a driver to use IMX6Q to receive image data from a CMOS chip(ev76c560), with 1280*1024 pixels, and the pixel clock is 114 MHz. I can read data from the chip pins by using  oscilloscope, but I can't read data from ipu. Is the width of the image data too big, or the frequency of the pixel clock too high?

0 Kudos
Reply
1 Reply

698 Views
joanxie
NXP TechSupport
NXP TechSupport

what data format and frame rate  do you set? for IPU capture throughput is 240M, when you capture data, any error message?

0 Kudos
Reply