Hi !
I am tring to design IMX6Q board.But something wrong.i set BOOT_MODE0 is 0 ,BOOT_MODE1 is 0,BOOT from fuses.It can be boot success.(But there is actually mistake,i meant to internal boot Mode).
so i change boot setting,BOOT_MODE0 is 1,BOOT_MODE1 is 0.but it does not boot success.
The general phenomenon is that after i set BOOT pin to boot from fuses(Boot success!),then i set BOOT pin to boot from internal Boot Mode,But the board can not boot properly.
so i wonder why.
thank you
Yacheng Zhang
已解决! 转到解答。
Sorry,There are mistakes in my word.In fact,i set BOOT_MODE0 is 0,BOOT_MODE1 is 1,It should be boot form internel,but it failed to boot.Then i try to set BOOT_MODE0 is 0,BOOT_MODE1 is 0,It should be boot from fuses,And it boot successfully.
So i want to know why failed boot from internel.
thanks