Dear *,
I have an IMX6 connected via AUD3 to interface 1 of WM8958, with MCLK on CLK2 and have the following configuration in device tree.
I would like to configure codec as SLAVE and SSI2 as master (and viceversa to test some other parts).
&i2c1 {
clock-frequency = <100000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c1>;
status = "okay";
codec: wm8958@1a {
compatible = "wlf,wm8958";
reg = <0x1a>;
clocks = <&clks 201>;
clock-names = "mclk1";
DBVDD1-supply = <&vgen3_reg>;
DBVDD2-supply = <&vgen3_reg>;
DBVDD3-supply = <&vgen3_reg>;
DCVDD-supply;
AVDD1-supply;
AVDD2-supply = <&vgen3_reg>;
CPVDD-supply = <&vgen3_reg>;
SPKVDD1-supply = <®_audio>;
SPKVDD2-supply = <®_audio>;
wlf,ldo1ena = <&gpio3 13 0>;
wlf,ldo2ena = <&gpio3 14 0>;
};
....
}
....
sound {
compatible = "fsl,imx6ul-ddr3-arm2-wm8958",
"fsl,imx-audio-wm8958";
model = "wm8958-audio";
cpu-dai = <&ssi2>;
audio-codec = <&codec>;
asrc-controller = <&asrc>;
audio-routing =
"Headphone Jack", "HPOUTL",
"Headphone Jack", "HPOUTR",
"Ext Spk", "SPKOUTL",
"Ext Spk", "SPKOUTR",
"MICBIAS", "AMIC",
"IN3R", "MICBIAS",
"DMIC", "MICBIAS",
"DMICDAT", "DMIC",
"CPU-Playback", "ASRC-Playback",
"Playback", "CPU-Playback",
"ASRC-Capture", "CPU-Capture",
"CPU-Capture", "Capture";
mux-int-port = <2>;
mux-ext-port = <3>;
//hp-det-gpios = <&gpio7 8 1>;
//mic-det-gpios = <&gpio1 9 1>;
//codec-master;
};
..
&ssi2 {
fsl,mode = "i2s-master";
status = "okay";
};
...
&audmux {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_audmux>;
status = "okay";
};
pinctrl_audmux: audmuxgrp {
fsl,pins = <
MX6QDL_PAD_CSI0_DAT7__AUD3_RXD 0x130b0
MX6QDL_PAD_CSI0_DAT4__AUD3_TXC 0x130b0
MX6QDL_PAD_CSI0_DAT5__AUD3_TXD 0x110b0
MX6QDL_PAD_CSI0_DAT6__AUD3_TXFS 0x130b0
MX6QDL_PAD_EIM_DA12__GPIO3_IO12 0x80000000
MX6QDL_PAD_GPIO_3__CCM_CLKO2 0x0001B0B0
>;
};
Now if I will try to play a sound (with tinyplay for wav or with stagefright for mp3), no BCLK/FS/DACDAT will be activate.
If I configure codec as master (uncommenting codec-master in sound) and i2s-master to i2s-slave in &ssi2, I will see BCLK,FS continuously but playing an audio file nothing happens on DACDAT (every time pulled-up).
Someone can help me, I'm not expert in device-tree, probably I forgot to configure some parts.
I try also codec-master with i2s-slave and i2s-master and without codec-master with i2s-slave and i2s-master, but not work.
Thank's
已解决! 转到解答。
I found the problem, is report it:
The problem is the audmux configuration, is possible to configure it in the device-tree or fix the driver in sound/soc/fsl/imx-wm8958.c where there are no configuration for audmux, I simply add
#include "imx-audmux.h"
and in imx_wm8958_probe after audio-codec
int int_port, ext_port;
...
if (!strstr(cpu_np->name, "ssi"))
goto audmux_bypass;
ret = of_property_read_u32(np, "mux-int-port", &int_port);
if (ret) {
dev_err(&pdev->dev, "mux-int-port missing or invalid\n");
return ret;
}
ret = of_property_read_u32(np, "mux-ext-port", &ext_port);
if (ret) {
dev_err(&pdev->dev, "mux-ext-port missing or invalid\n");
return ret;
}
/*
* The port numbering in the hardware manual starts at 1, while
* the audmux API expects it starts at 0.
*/
int_port--;
ext_port--;
ret = imx_audmux_v2_configure_port(int_port,
IMX_AUDMUX_V2_PTCR_SYN |
IMX_AUDMUX_V2_PTCR_TFSEL(ext_port) |
IMX_AUDMUX_V2_PTCR_TCSEL(ext_port) |
IMX_AUDMUX_V2_PTCR_TFSDIR |
IMX_AUDMUX_V2_PTCR_TCLKDIR,
IMX_AUDMUX_V2_PDCR_RXDSEL(ext_port));
if (ret) {
dev_err(&pdev->dev, "audmux internal port setup failed\n");
return ret;
}
imx_audmux_v2_configure_port(ext_port,
IMX_AUDMUX_V2_PTCR_SYN,
IMX_AUDMUX_V2_PDCR_RXDSEL(int_port));
if (ret) {
dev_err(&pdev->dev, "audmux external port setup failed\n");
return ret;
}
audmux_bypass:
...
Thank's
Hi Cristian Sicilia,
I working same chip on Android6.0 . In this Mic is not working, headphone output is very low.
Can you give suggestion on this.
Regards,
Aravinth
Try with tynimix from command line, the BOOST tipically resolve the problem with speaker outout volume.
Recording could be a problem in selection the ritght path of codec (probably you hear from IN1 of codec and mic is on IN2 for example), you will resolve this with tinymix at runtime from command line (then you can change default setting).
Regards
In my schematic, the headset was on LEFT and the Speaker was on RIGHT ouput.
Now with tinymix you can set to OFF LEFT and ON RIGHT (and viceversa), then you can control in this way the Headset and Speacker (in the same way with the input).
So you can manage the output (and input) in the same way if it is a speaker, headset, generic aux, etc.
Thank you for support,
I have check the configuration, but I don't see the problem.
I see different thing, like
ssi2: ssi@0202c000
but it seems already declared in imported dts, so I suppose that is not required, in any case from debug runtime data I found the ssi on 202c000 (SSI2).
The strange thing is that when I play a sound (in codec-master mode) the SSI don't generate DACDAT data, but remain pulled HIGH, like when it is configured to another out port.
This is the output from audmux, the strange thing (from my point of view) are:
1. in "<---ssi1" that should be the ssi2 in device tree, is connected with SSI5 (I expected SSI3 !?)
2. in "<--- ssi3" I don't see connection, I will expect that it is connected with ssi1
Probably I lost some step, but seems that the problem is in the audmux configuration.
# cat /sys/kernel/debug/audmux/ssi*
PDCR: 0000a000 <--- ssi0
PTCR: ad400800
TxFS output from SSI6, TxClk output from SSI6
Port is symmetric
Data received from SSI6
PDCR: 00008000 <--- ssi1
PTCR: a5000800
TxFS output from SSI5, TxClk output from SSI5
Port is symmetric
Data received from SSI5
PDCR: 00006000 <--- ssi2
PTCR: 9cc00800
TxFS output from SSI4, TxClk output from SSI4
Port is symmetric
Data received from SSI4
PDCR: 00004000 <--- ssi3
PTCR: 00000800
TxFS input, TxClk input
Port is symmetric
Data received from SSI3
PDCR: 00002000 <--- ssi4
PTCR: 00000800
TxFS input, TxClk input
Port is symmetric
Data received from imx-ssi.1
PDCR: 00000000 <--- ssi5
PTCR: 00000800
TxFS input, TxClk input
Port is symmetric
Data received from imx-ssi.0
PDCR: 0000c000 <--- ssi6
PTCR: 00000800
TxFS input, TxClk input
Port is symmetric
Data received from UNKNOWN
I found the problem, is report it:
The problem is the audmux configuration, is possible to configure it in the device-tree or fix the driver in sound/soc/fsl/imx-wm8958.c where there are no configuration for audmux, I simply add
#include "imx-audmux.h"
and in imx_wm8958_probe after audio-codec
int int_port, ext_port;
...
if (!strstr(cpu_np->name, "ssi"))
goto audmux_bypass;
ret = of_property_read_u32(np, "mux-int-port", &int_port);
if (ret) {
dev_err(&pdev->dev, "mux-int-port missing or invalid\n");
return ret;
}
ret = of_property_read_u32(np, "mux-ext-port", &ext_port);
if (ret) {
dev_err(&pdev->dev, "mux-ext-port missing or invalid\n");
return ret;
}
/*
* The port numbering in the hardware manual starts at 1, while
* the audmux API expects it starts at 0.
*/
int_port--;
ext_port--;
ret = imx_audmux_v2_configure_port(int_port,
IMX_AUDMUX_V2_PTCR_SYN |
IMX_AUDMUX_V2_PTCR_TFSEL(ext_port) |
IMX_AUDMUX_V2_PTCR_TCSEL(ext_port) |
IMX_AUDMUX_V2_PTCR_TFSDIR |
IMX_AUDMUX_V2_PTCR_TCLKDIR,
IMX_AUDMUX_V2_PDCR_RXDSEL(ext_port));
if (ret) {
dev_err(&pdev->dev, "audmux internal port setup failed\n");
return ret;
}
imx_audmux_v2_configure_port(ext_port,
IMX_AUDMUX_V2_PTCR_SYN,
IMX_AUDMUX_V2_PDCR_RXDSEL(int_port));
if (ret) {
dev_err(&pdev->dev, "audmux external port setup failed\n");
return ret;
}
audmux_bypass:
...
Thank's