IMX6 Solo Lite Custom board Pin Multiplexing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 Solo Lite Custom board Pin Multiplexing

1,037 Views
satyavenkatasan
Contributor I

Dear Freescale,

We are using the IMX6 Solo lite Processor in our design. Using the iomux_tool_v3.4.0.3 we selected the peripherals & pin functionality in the tool and generated the pin muxing .c & .h files. Know I wanted to patch with the IMX6Sl evk 3.0.35 version kernel. hear I have 2 questions is it possible to patch the files that got generated directly. if it so, suggest me the steps. if direct patching is not possible suggest me how can i use this files in detail.

Thanks & regards,

Satya Venkata Sandeep A.

Labels (3)
0 Kudos
Reply
1 Reply

635 Views
igorpadykov
NXP Employee
NXP Employee

Hi satya

there is no currently an automated way to transfer a design from iomux

files to linux. One can edit linux files manually using

Chapter 2 Configuring the IOMUX Controller  attached Porting Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply