Hello Atilla,
Yes, the i.MX6 Quad/Dual and Solo Lite are Pin a Pin Compatible and Software Compatible. This is one of the advantages of the i.MX6 Family.
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Jaime,
Just to clarify, IMX6Quad, IMX6Dual, IMX6DualLite, IMX6Solo and IMX6 SoloLite are all pin compatible? Not just
IMX6Q-D-S within each other and IMX6DL-SL witihin each other independently?
Thanks,
Mete
Hi,
As per datasheet "For Quad core system, connect to VDD_ARM_IN. For Dual core system, may be shorted to GND together with
VDD_ARM23_CAP to reduce leakage." Now I have made a design with Quad core and i would like to replace with Dual core and I have connected VDD_ARM23_IN with VDD_ARM_IN, and I havn't put an option for connecting with GND.
What should i do now?
What are the other changes i need to do while to have compatibility for Dual core and Quad core?
Regards,
Mrudang