IMX6 DL: Which version of Vivante VAnalyzer do i need?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 DL: Which version of Vivante VAnalyzer do i need?

Jump to solution
2,367 Views
jeroen-verfailie
Contributor I

Hey There!

We are developing a gstreamer pipeline, and trying to offload some work to the GPU.
To profile this, we're trying to use the gpuProfiler of the galcore module.

The *.vpd files are being generated (I attached one) and do seem to contain data.

The problem is that the VivanteIDE doesn't seem to recognise the files as a valid format. I've also tried with some earlier versions I've found in the NXP repositories, but all refused to show any gpu data.

Some information:
GPU: Vivante GC880 / revision="5.1.0_rc6"
OpenGL ES 3.0
Linux version: 5.4.70-F+S
VivanteIDE version:  5.2.0
All build with yocto 3.0.4 (Zeus)

 

Thanks in advance!

Labels (1)
0 Kudos
Reply
1 Solution
2,274 Views
joanxie
NXP TechSupport
NXP TechSupport

gputop is good tools, you also can refer to the chapter 14 GPU Tools of enclosed file

View solution in original post

6 Replies
2,341 Views
joanxie
NXP TechSupport
NXP TechSupport

normally we will suggest customer to use the latest version, but I also have another solution from the customer who has the similar issue, they open the vpd file with an notepad++ or viAnd change the text VP2010 in VP12 save it, then can read it correctly, maybe you can try it

0 Kudos
Reply
2,333 Views
jeroen-verfailie
Contributor I

Dear Joanxie

 

Thank you for the information.
The changing of the VP2010 -> VP12 does seems to change behaviour, although now i get a 'No frame data in profiled data file' error. Any idea why that would happen?

The *vpd file is automatically generated whilst starting gstreamer.
These were the exported vars:

export VIV_PROFILE=1
export VP_FRAME_NUM=20
export V_SYNC_MODE=1

Both gpuProfiler=1 and powerManagement=0 in the galcore module.

Thanks!

0 Kudos
Reply
2,321 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
2,300 Views
jeroen-verfailie
Contributor I

Hey Joanxie

Sorry for the late response.

I did test it with the latest IDE, unfortunately without success.
In the meantime, I've used other tools such as gputop to do some basic profiling.
If you have any more ideas i'd happily test them, although gputop is good enough for my use case.

Thanks for your help!

0 Kudos
Reply
2,275 Views
joanxie
NXP TechSupport
NXP TechSupport

gputop is good tools, you also can refer to the chapter 14 GPU Tools of enclosed file

2,275 Views
joanxie
NXP TechSupport
NXP TechSupport

gputop is good tools, you also can refer to the chapter 14 GPU Tools of enclosed file

0 Kudos
Reply