IMX6 3.0.35 : parrallel input video doesn't work in BT656 mode (ADV7401)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 3.0.35 : parrallel input video doesn't work in BT656 mode (ADV7401)

1,625 Views
pchevalier
Contributor I

Hello,

I try to implement a driver of ADV7401 based on ADV7180

I can get a video (very poor quality but it work) in GATED_MODE (p->u.bt656.clock_curr = 27000000;)

but i want to be in BT656 mode (p->u.bt656.clock_curr = 0;)

I have check the frames with scope all EAV/SAV code are OK.

When i am in BT656 mode, when i launch gstreamer i have a timeout error :

v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0

Does Interlaced BT656 mode work for kernel 3.0.35 ?

Thanks for your help !

Pierre

Labels (3)
0 Kudos
Reply
3 Replies

993 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

993 Views
pchevalier
Contributor I

No sorry it don't work...

0 Kudos
Reply

993 Views
igorpadykov
NXP Employee
NXP Employee

One can also try SDK (it has test for ADV7180)

i.MX 6Series Platform SDK : Bare-metal SDK

0 Kudos
Reply