Hi All ,
I am trying to enable pcie. I am trying this on i.Mx6Q sabreauto with SCH-27142-REV C.
As i have browsed on forum and found that this board should support pcie. But i am getting following error!!
iMX6 PCIe PCIe RC mode imx_pcie_pltfm_probe entering.
PCIE: imx_pcie_pltfm_probe start link up.
link up failed, DB_R0:0x001f3e00, DB_R1:0x08200000!
IMX PCIe port: link down!
I have used L3.0.35_4.1.0_130816_source.tar.gz.
pcie device is of Atheros.
what could be the possible reason for this issue?
Regards ,
Hare Krishna
Hi Hare
first I would suggest to test verified devices described in attached Linux Manual
sect.35.4 Using PCIe Endpoint and running Tests.
As for atheros pcie suggest to check link
i.MX6Q PCIe EP/RC Validation System
and verify software settings and that card has sufficient power current
CONFIG_IMX_PCIE=y
# CONFIG_IMX_PCIE_EP_MODE_IN_EP_RC_SYS is not set
# CONFIG_IMX_PCIE_RC_MODE_IN_EP_RC_SYS=y
Also for fail detection one can try attached patches.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------