I2c chip Driver for Audio Amp & AM/FM tuner in I.MX28 linux BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2c chip Driver for Audio Amp & AM/FM tuner in I.MX28 linux BSP

ソリューションへジャンプ
1,916件の閲覧回数
srinivasanshanm
Contributor III

Hi,

As am newbiee to this I.mx28 BSP's , & new to audio amp & AM/FM tuner, I found there are no drivers for audio amplifier ( TDA7563B Audio Amp) & (Si4743 AM/FM tuner ) interfaced through i2c in L2.6.35_10.12.01_ER_source, could you pls let me know how to get started with it or if we have any other drivers for the same,

Thanks in advance,

ラベル(2)
0 件の賞賛
返信
1 解決策
1,348件の閲覧回数
PeterChan
NXP Employee
NXP Employee

On i.MX28 EVK, the audio codec is SGTL5000 where the control is also via I2C interface. It is enabled by default in Linux BSP. You may port the TDA753B driver by taking the SGTL5000 as the reference. Please also check your vendor if they already have linux driver code for their chips.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,348件の閲覧回数
srinivasanshanm
Contributor III

Could anybody please kindly let me know any information on the basics of Audio amp & atleast any drivers available for audio amplifier in Linux o that it can be ported to TDA753B by having that driver as the reference

Awaiting for your replies,

Thanks in advance

0 件の賞賛
返信
1,348件の閲覧回数
YixingKong
Senior Contributor IV

Srinivasan, could you please click Corret Answer/Helpful Answer, if your question had been answered?

Thanks,

Yixing

0 件の賞賛
返信
1,348件の閲覧回数
srinivasanshanm
Contributor III

Ya.. Thanks a lot for your support , it gave me an idea.. would be working on the same .........

You can close this thread...

Once again Many Many Thanks,

0 件の賞賛
返信
1,349件の閲覧回数
PeterChan
NXP Employee
NXP Employee

On i.MX28 EVK, the audio codec is SGTL5000 where the control is also via I2C interface. It is enabled by default in Linux BSP. You may port the TDA753B driver by taking the SGTL5000 as the reference. Please also check your vendor if they already have linux driver code for their chips.

0 件の賞賛
返信