I.MX6qP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6qP

1,808 Views
manishUniyal
Contributor I

Hello Everyone,

I have to write bootz ${loadaddr} - ${fdt_addr} everytime while booting linux in I.MX6QP sabre board.

Can Anyone provide solution that how can I resolve this issue. Or How can i boot my board directly without entering this command again and again.

I would be thankful in this regards.

Thanks

0 Kudos
Reply
3 Replies

1,782 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using the NXP I.MX6QP sabre board? Which version BSP are you using?

0 Kudos
Reply

1,779 Views
manishUniyal
Contributor I

Yes I am using NXP I.MX6QP sabre board.

I have downloaded the demo file Linux 5.15.32_2.0.0​.

0 Kudos
Reply

1,774 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You need to add it to the U-boot source code, You can modify the default environment variables on the configuration header file.

0 Kudos
Reply