Hello NXP,
I am able to update and run the firmware's using DFU. Which are less than 196kb as the DFU using the ITCM region which is of size 256kb.
following this Unable to update the Firmware through DFU - NXP Community
The problem is when I try to update the firmware that is greater than the 196kb it is getting failed due to the lack of memory in that region.
Is there any to increase the ITCM region size keeping the DTCM as 256kb?
or
Is there any alternative way to download and run the applications greater than 1Mb using DFU?
Thanks in advance for the help.
Regards,
Ragnar.
HI @AldoG ,
Using the DFU example provided in the SDK I could be able to update and run the application by writing the application downloaded to the ITCM to flash region and jumping to it.
But when I tried to write the downloaded application directly to flash instead of following the above process
my bootloader is unable to set the stack pointer when application jump is performed and immediately returning to the boot loader.
could you please help me with this case?
Thanks & Regards,
Ragnar.