Hello,
From the iMX Machine Learning Guide:
https://www.nxp.com/docs/en/user-guide/IMX-MACHINE-LEARNING-UG.pdf
When I am running benchmarks for TFLite models, there is an option --nnapi=true
How do I know when the inference is being done by the GPU and the NPU?
Thanks
Solved! Go to Solution.
To run the inference using the GPU/NPU hardware accelerator, add the --use_nnapi=true command line argument:
For NPU: adb shell /data/local/tmp/benchmark_model --graph=/data/local/tmp/mobilenet_v2_1.0_224_quant.tflite --use_nnapi=true --nnapi_accelerator_name=vsi-npu
For GPU: adb root adb shell setprop vendor.USE_GPU_INFERENCE 1 adb shell /data/local/tmp/benchmark_model --graph=/data/local/tmp/mobilenet_v2_1.0_224_quant.tflite --use_nnapi=true
more detailed information, you can refer to the link as below,
"https://www.nxp.com/docs/en/user-guide/IMX_ANDROID_TENSORFLOWLITE_USERS_GUIDE.pdf"
To run the inference using the GPU/NPU hardware accelerator, add the --use_nnapi=true command line argument:
For NPU: adb shell /data/local/tmp/benchmark_model --graph=/data/local/tmp/mobilenet_v2_1.0_224_quant.tflite --use_nnapi=true --nnapi_accelerator_name=vsi-npu
For GPU: adb root adb shell setprop vendor.USE_GPU_INFERENCE 1 adb shell /data/local/tmp/benchmark_model --graph=/data/local/tmp/mobilenet_v2_1.0_224_quant.tflite --use_nnapi=true
more detailed information, you can refer to the link as below,
"https://www.nxp.com/docs/en/user-guide/IMX_ANDROID_TENSORFLOWLITE_USERS_GUIDE.pdf"
I would also like to know how to verify that I am running inference on the NPU vs. the GPU.
I have my own scripts and have attempted to run inference on a set of models using the USE_GPU_INFERENCE environment variable. I am using TensorFlow Lite and the VX delegate on the i.MX 8M Plus evaluation kit with the Linux v5.15.32-2.0.0 image. The results that I am getting are so remarkably similar (warmup times within 2-3 ms of each other and inference times within 0.01 ms of each other on average) that I am skeptical that they are running on different accelerators.
How can I make sure that I'm actually using both devices? Thank you.
Thank you joanxie for clarification.
I have one more question.
I am trying to access this link:
https://community.nxp.com/community/eiq/blog/2019/07/15/eiq-sample-apps-tflite-quantization
Do you know if there is a similar link?
Thanks in advance
I got "Page not found", I don't know what this is
Hello,
It is the quantization guide for the eIQ Sample Apps from here
https://community.nxp.com/t5/eIQ-Machine-Learning-Software/eIQ-Sample-Apps-Overview/ta-p/1122925
Is there a similar link to the broken one?
Thanks and regards.