Hi
My platform is Linux on i.mx8mp-evk.
I am currently executing:
$echo 38 > /sys/class/gpio/export
$echo out > /sys/class/gpio/gpio38/direction
I can successfully control M.2's pin 56, W_DISABLE1, which is PCIe_nDIS,
Now, I want to control BT disable, which is M.2's pin 54, W_DISABLE2.
Which GPIO pin should I set?
Thanks!
Hi Chavira
Thans for your reply,
I had tried to execoute gpioset EXP_P0_7 , but it shows
Then I tried to execute
Hi @ChChang!
I modify the device tree to use the gpio more easily.
Sorry for the mistake!
You should use the command:
gpioset -c gpiochip5 7=1
And
gpioset -c gpiochip5 7=0
You can measure pin 22 of the expansion header of the board as the same gpio of the m.2 connector.
Best Regards!
Chavira
Hi! @ChChang!
What BSP are you using?
Yes, you have to solder the resistor "R142", if you see in the schematic the resistor "R142" is not soldered, in consequence, the iMX pin is not connected to the TEST POINT.
Best Regards!
Chavira
Hi @ChChang!
According to the Schematic, the value of Resistor R142 is 0 Ohm.
Watching the datasheet of the wifi module I noticed that is not the correct pin to turn off the wifi module pin 56 of the m.2 connector is the correct one to turn off the wifi module.
https://www.azurewave.com/img/nxp/AW-CM276MA-PUR_DS_B3_H_STD.pdf
On our device tree is defined as a regulator
https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mp-evk.dts#L66
If you want to control manually the wifi module you should change the device tree and control it like gpio.
Best Regards!
Chavira
Hi Chavira
My BSP version is L5.15-kirkstone
I also tried directly connecting EXP_P0_7 to TP39 with a wire, but it doesn't affect BT working.
Can only soldering R142 work?
Thanks for yor reply!
Regards,
CH
Hi @ChChang!
Thank you for contacting NXP Support!
That pin is connected to the IO expander.
You can control that gpio using the "gpioset" command.
You should use "gpioset EXP_P0_7=1" or "gpioset EXP_P0_7=0" to control that pin.
Best Regards!
Chavira