Dear all
I use i.mx6Q (Part numbers D) and have a Question about " 50.7.4 Digital Regulator Core Register".
PMU_REG_COREn :
Address: 20C_8000h base + 140h offset + (4d × i), where i=0d to 3d
That is...
① 0x020C8140
② 0x020C8144
③ 0x020C8148
④ 0x020C814C
But,
I can set value to ①and② , but I can't set the values to ③and④.
I set the value to ①、then ②,③and④ register is set to the same value as ①.
Is this a correct setting to set the only ① register ?
Thanks for your help,
Nomusan
Thank you ,Igorpadykov.
There is additional information.
Look at the following differences,please.
-Processor Reference Manual Rev.3.
PMU_REG_COREn Address: 20C_8000h base + 140h offset
-Processor Reference Manual Rev.4
PMU_REG_COREn Address: 20C_8000h base + 140h offset + (4d × i), where i=0d to 3d
Three addresses have been added from the new revision.
I can read register value each of them, but I can write only ① and ② address.
Actually, if I set one, all four have the same value.
Do you think that one setting is enough and that it is a mistake to set four?
Hi yutaka
seems there is one ldo as described in sect.50.2 Digital LDO Regulators
i.MX6DQ Reference Manual :
"The three digital regulators are known as LDO_ARM, LDO_PU, and LDO_SOC."
check also power connections in Figure 50-1. Power system overview
http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, igor and yutaka
I met a same issue.
Can different voltage values be applied to different CPU core? Alternatively, even if I can configure 4 registers of PMU_REG_CORE, actually only the first register takes effect?
Thanks and Regards
Zinan