How to rotate a mp4 video with gstreamer in i.mx6 SABRE Lite

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to rotate a mp4 video with gstreamer in i.mx6 SABRE Lite

7,186件の閲覧回数
wilsonmak
Contributor I

I am trying to rotate a video clockwise with gplay command line.

But it got errors:

[Playing  ][Vol=01][00:00:05/00:02:22][fps:29]t

Set rotation between 0, 90, 180, 270: 90

fsl_player_rotate(): AutVideoSinko=videosink : ActualVideoSink=videosink-actual-sink-mfw_v4l

rotate_value = 90

rotate = 90update_mfw_v4lsink_parameter(): Update mfw_v4lsink successfully!

fsl_player_rotate(): After rotate_value == 90

mxc_v4l2_output mxc_v4l2_output.0: vout check task failed

full screen size:1920x1080

Failed to initalize the dispmxc_ipu mxc_ipu: ERR: no-0x0,ipu_queue_task err:-22

lay

mxc_v4l2_output mxc_v4l2_output.0: display work fail ret = -22

But it's fine to rotate 180, but 90 and 270.


And I try the following to rotate by 90:

gst-launch filesrc location=/data/No5.mp4 typefind=true ! videoflip method=clockwise ! aiurdemux ! vpudec ! mfw_v4lsink

Errors again:

MFW_GST_V4LSINK_PLUGIN 3.0.7 build on Nov 11 2013 00:17:51.

WARNING: erroneous pipeline: could not link videoflip0 to aiurdemux0


What is the best way to rotate a video in i.mx6 and how?

Thanks,

Wilson

ラベル(1)
タグ(2)
0 件の賞賛
返信
6 返答(返信)

3,136件の閲覧回数
wilsonmak
Contributor I

1) Rotation of 180 is fine

gst-launch filesrc location=/home/media/bbb_short_1080p.avi typefind=true ! ai

urdemux ! vpudec ! mfw_v4lsink rotate=180

Console dump

===========

MFW_GST_V4LSINK_PLUGIN 3.0.8 build on Dec 12 2013 07:15:06.

rotate = 180Setting pipeline to PAUSED ...

[INFO]  Product Info: i.MX6Q/D/S

vpudec versions :smileyhappy:

        plugin: 3.0.8

        wrapper: 1.0.38(VPUWRAPPER_ARM_LINUX Build on Dec 12 2013 07:14:31)

        vpulib: 5.4.15

        firmware: 2.3.10.40778

Pipeline is PREROLLING ...

Aiur: 3.0.8

Core: AVI_PARSER_03.05.07  build on Jul  3 2013 01:47:35

  mime: video/x-msvideo

  file: /usr/lib/imx-mm/parser/lib_avi_parser_arm11_elinux.so.3.1

Content Info:

        URI:

              file:///home/media/bbb_short_1080p.avi

        Idx File:

              /root/.aiur/.home.media.bbb_short_1080p.avi.aidx

        Seekable  : Yes

        Size(byte): 32335220

Movie Info:

        Seekable  : Yes

        Live      : No

        Duration  : 0:00:30.752000000

        ReadMode  : File

        Track     : 2

Track 00 [video_000000] Enabled

        Duration: 0:00:30.750000000

        Language: und

        Mime:

              video/mpeg, mpegversion=(int)4, parsed=(boolean)true, width=(int)1920, height=(i

              nt)1080, framerate=(fraction)24/1

Track 01 [audio_000000] Enabled

        Duration: 0:00:30.752000000

        Language: und

        Mime:

              audio/x-ac3, channels=(int)5, rate=(int)48000, bitrate=(int)448000, framed=(bool

              ean)true

[INFO]  bitstreamMode 1, chromaInterleave 1, mapType 0, tiled2LinearEnable 0

set v4l rotate sucessfully

>>V4L_SINK: Actually buffer status:

        hardware buffer : 10

        software buffer : 0

Pipeline is PREROLLED ...

Setting pipeline to PLAYING ...

full screen size:1920x1080

[V4L Update Display]: left=0, top=0, width=1920, height=1080

set v4l display crop sucessfully

New clock: GstSystemClock

=====================================================================

Rotation of either 90 or 270 is not good

Console Dump

============

gst-launch filesrc location=/home/media/bbb_short_1080p.avi typefind=true ! ai

urdemux ! vpudec ! mfw_v4lsink rotate=90

MFW_GST_V4LSINK_PLUGIN 3.0.8 build on Dec 12 2013 07:15:06.

rotate = 90Setting pipeline to PAUSED ...

[INFO]  Product Info: i.MX6Q/D/S

vpudec versions :smileyhappy:

        plugin: 3.0.8

        wrapper: 1.0.38(VPUWRAPPER_ARM_LINUX Build on Dec 12 2013 07:14:31)

        vpulib: 5.4.15

        firmware: 2.3.10.40778

Pipeline is PREROLLING ...

Aiur: 3.0.8

Core: AVI_PARSER_03.05.07  build on Jul  3 2013 01:47:35

  mime: video/x-msvideo

  file: /usr/lib/imx-mm/parser/lib_avi_parser_arm11_elinux.so.3.1

Content Info:

        URI:

              file:///home/media/bbb_short_1080p.avi

        Idx File:

              /root/.aiur/.home.media.bbb_short_1080p.avi.aidx

        Seekable  : Yes

        Size(byte): 32335220

Movie Info:

        Seekable  : Yes

        Live      : No

        Duration  : 0:00:30.752000000

        ReadMode  : File

        Track     : 2

Track 00 [video_000000] Enabled

        Duration: 0:00:30.750000000

        Language: und

        Mime:

              video/mpeg, mpegversion=(int)4, parsed=(boolean)true, width=(int)1920, height=(i

              nt)1080, framerate=(fraction)24/1

Track 01 [audio_000000] Enabled

        Duration: 0:00:30.752000000

        Language: und

        Mime:

              audio/x-ac3, channels=(int)5, rate=(int)48000, bitrate=(int)448000, framed=(bool

              ean)true

[INFO]  bitstreamMode 1, chromaInterleave 1, mapType 0, tiled2LinearEnable 0

set v4l rotate sucessfully

>>V4L_SINK: Actually buffer status:

        hardware buffer : 10

        software buffer : 0

Pipeline is PREROLLED ...

Setting pipeline to PLAYING ...

full screen size:1920x1080

[V4L Update Display]: left=0, top=0, width=1920, height=1080

set v4l display crop sucessfully

New clock: GstSystemClock

=============================================================

P.S.  There is no video shown on the screen.

Thanks,
Wilson

0 件の賞賛
返信

3,136件の閲覧回数
xizhouwang
Contributor II

Hi Wilson

I'm facing the same issue on a i.MX6D board. It seems related to the IPU setting. No 90 or 270 rotation for a video play back. Audio is OK. No video shown but the Penguin logo still in place.

Using  echo 1 > /sys/class/graphics/fb0/rotate is not working while echo 2  will rotate the whole display 180 degrees.

Also tried the latest FSL gst libs, results are the same.

Any workaround found?

Thanks,  X Wang

0 件の賞賛
返信

3,136件の閲覧回数
wilsonmak
Contributor I

Hi X Wing,

You can resize the width and height first and then rotate the video by 90 or 270.

But still I have problem showing the portrait video 720x1280.

For example,

> gplay abc.mp4

> z 0 0 720 1280

> t = 90 (rotate by 90)

However, with these settings, the video can't be shown in FULL SCREEN after rotation. 

Thanks,

Wilson

0 件の賞賛
返信

3,136件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Wilson,

Which BSP are you using?

Best Regards

Dan

0 件の賞賛
返信

3,136件の閲覧回数
wilsonmak
Contributor I

Hi Dan,

I am using Timesys BSP.

The kernel is 3.0.35-ts-armv7l.

Thanks,

Wilson

0 件の賞賛
返信

3,136件の閲覧回数
LeonardoSandova
Specialist I

There is a property (rotate) on the mfw_v4lsink element, can you try it?

0 件の賞賛
返信