How to generate interrupt INT7 in GPIO1?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to generate interrupt INT7 in GPIO1?

3,634件の閲覧回数
Markon
Contributor II

I need individual interrupt from pad GPIO_7. I configured registers connected with GPIO, IOMUXC - similar as in Interrupts with GPIO1 INT0-7 , and GIC registers. When I have interrupt handler bounded with IRQ 98, it works. When I have interrupt handler bounded with IRQ 90, it doesn't work. According to i.MX 6Dual/6Quad Applications
Processor Reference Manual, GPIO_7, ARM processor should receive also individual interrupt from GPIO_7.

How to configure iMX6Q to reveive individual interrupt, IRQ 90 ?

0 件の賞賛
返信
3 返答(返信)

3,320件の閲覧回数
b36401
NXP Employee
NXP Employee

Please refer chapter 3.2.4 "Interrupt Source Code Structure" of i.MX Linux Reference Manual.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,320件の閲覧回数
Markon
Contributor II

I'm not good in Linux. I work on FreeRTOS and I'm looking for solution connected close to hardware.

0 件の賞賛
返信

3,320件の閲覧回数
Yuri
NXP Employee
NXP Employee
0 件の賞賛
返信