Hello,
I am a new developer on i.MX6Q-AI and now using Freescale YOCTO BSP r14.10.28.
I have three boards on my hand:
The problem is:
I got the Atheros ETH phy running well on CPU board and tested with another set of phy and cpuboard.
But when I connect Broadcom ETH phy to CPU board, it doesnot work properly.
I have tried to include ETH drive in kernel with the cmd "make menuconfig" and find that there is no driver for Broadcom 89810.
What can I do to enable the Broadcom ETH phy?
Thanks and regards
Jerry
Hello,
I hope the following helps.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,Y uri
Happy new year!
The firmware seems support only the bcm 4seri es wifi chips and do not include driver for bcm89810.
Any other suggestions for me?
Much thanks