Hello,
This is on the i.MX6. We've have had some success implementing the webcam gadget in our application, but we don't know how to detect when the device is unplugged from the host.
If the host-side application stops streaming, we can unplug from USB, re-plug in to USB and start streaming again, all without disturbing the main application running in Linux.
The problem occurs if the user disconnects the camera from the host without stopping video and then reconnects and tries to start video streaming again. Our application freezes, and sometimes the kernel crashes. If we had a way to detect that the device is unplugged from the host, we could probably take appropriate action to shut down streaming in an orderly manner. Is there a way to do this?
Thanks very much,
Ed Pearson
已解决! 转到解答。
Hi Ed
one can try to test USBPHYx_STATUS regsiter, please
check sect.66.2.4.4 HS Disconnect Detector, USB Plugged-In Detector,
i.MX6DQ Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ivan,
I have one more question.
We tried detecting that the device is disconnected by detecting when it has stopped receiving SOFs. We the steps to do this were:
The idea being, if the SOF count stops incrementing we have a disconnect event and can respond appropriately.
What we've found is that, for about 30 seconds after disconnecting from the host, we continue to receive SOF interrupts. After about 30 seconds, something calls fsl_pullup with is_on == 0, and we stop receiving interrupts, and uvc_function_disable() is called. (I am not certain of the exact order of events, I'm relying on printk() statements to trace through all this.)
This happens even if the application is not loaded.
I'm told (but can't verify) that the embedded hub will stop sending SOFs immediately on disconnection from the host. If this is true can you think of anything that might explain the behavior that I'm seeing?
Thanks very much for all the help.
Regards,
Ed Pearson
Hi Ed
I am afraid with hub this may not work.
Unfortunately I am not aware of methods detecting
disconnection using high level OS APIs of usb driver, sorry.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Can you please check this code and make sure that I'm doing this correctly? It should print a message to the console when the state of the plug changes. I see nothing when I plug or unplug; either I am not addressing the register correctly, or there is something else wrong. Thanks very much.
Regards,
Ed Pearson
u32 get_plugin_status(void)
{
static u32 plug_status = 0;
void __iomem *phy_reg = MX6_IO_ADDRESS(USB_PHY0_BASE_ADDR);
u32 status = fsl_readl(phy_reg+HW_USBPHY_STATUS);
status &= BM_USBPHY_STATUS_DEVPLUGIN_STATUS;
if (status != plug_status)
{
plug_status = status; // report change in status to console?
printk("WEBCAM: plug_status changed to %d\n",plug_status);
}
if (status != 0)
return 1;
else
return 0;
}
Hi Ed
one can try to test USBPHYx_STATUS regsiter, please
check sect.66.2.4.4 HS Disconnect Detector, USB Plugged-In Detector,
i.MX6DQ Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thanks very much for the prompt reply. Our customer's design includes an onboard hub, connecting both the USB PHY and another USB peripheral to the host, so that an unplug would not be seen directly by the PHY. I'm a USB newbie, and don't know whether or not an unplug event would be reflected to the PHY. Do you happen to know if this is the case? If it is, then I'm all set. If not, I need to keep digging.
Thanks,
Ed