Hi all,
I Need to configure the 4GB micron eMMC device .
How to test the read and write in eMMC blocks,Based on the temperature changes durung the continuous
block read/write eMMC will effecting or not.
1.eMMC integration in kernel level,what are all changes i want to make it as to working condition of eMMC.
2.eMMC API's call to check the eMMC read /write cycle of eMMC block memory tten data.
3.eMMC partition and formatting commands
fdisk--> this is command correcrt for to fprmat the eMMC device.
dd--> read /write purpose dd command is correct or not
Thanks by,
Venkat
Hi Venkatesh
i.MX6 sd/mmc host driver implements a standard Linux driver interface to
the ultra MMC/SD host controller (uSDHC) .
Host driver is part of the Linux kernel MMC framework.
You can download Ubuntu for i.MX6 below and work with eMMC as
on PC Ubuntu computer
L3.0.35_4.1.0_UBUNTU_RFS_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,
i.MX 6Solo and i.MX 6Sololite Linux File System for the Ubuntu Images.
L3.0.35_4.1.0_DEMO_IMAGE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,
i.MX 6Solo and i.MX 6Sololite Linux Binary Demo Files.
One can check documentation in L3.0.35_4.1.0_LINUX_DOCS
Just for reference check sect.Chapter 8 Using a Linux Host to Set Up an SD/MMC Card
attached i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf - it shows
operations with partitions and blocks.
For APIs one can look below
kernel/git/cjb/mmc-utils.git - Userspace tools for MMC/SD devices.
[PATCH 1/1] mmc: User Application for testing SD/MMC Commands and extr
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------