I made a testing about 1000M ethernet maximum speed on toradex imx6q evaluation board. The board use KSZ8031 phy chip. Did anyone know faster ethernet speed on imx6q chip.
Hello,
From erratum ERR004512 (ENET: 1 Gb Ethernet MAC (ENET) system limitation) :
"Limitation of ENET throughput to around 400 Mbps. ENET remains fully compatible to
1Gb standard in terms of protocol and physical signaling. If the TX and RX peak data rate is higher
than 400 Mbps, there is a risk of ENET RX FIFO overrun".
http://www.nxp.com/assets/documents/data/en/errata/IMX6DQCE.pdf
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you