How do I enable the SJC Fuse i.mx8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I enable the SJC Fuse i.mx8

302件の閲覧回数
BruceGraham
Contributor I

How do I enable the SJC Fuse i.mx8

I assume it uses the uboot fuse command.

How do I determine the parameters?

 

0 件の賞賛
返信
2 返答(返信)

218件の閲覧回数
BruceGraham
Contributor I

Please provide a document #, and possibly a section # that explains the bit fields in the registers.
Thanks.

0 件の賞賛
返信

276件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

SJC enabled would mean that JTAG is enabled? It's already enabled.

In i.MX 8/8X family, the system JTAG controller (SJC) provides a method of regulating the JTAG access.
SJC provides the following security levels:

  • JTAG disabled – JTAG use is permanently blocked.
  • No-debug – JTAG security sensitive features are permanently blocked.
  • Secure JTAG – JTAG use is restricted (as in the no-debug level) unless a secret-key challenge/response
    protocol is successfully executed.
  • JTAG enabled – JTAG use is unrestricted.

The index and bit are 5[0]  and 22, you can refer to this article for fuse programming.

Regards

0 件の賞賛
返信