Hi all,请帮忙解答问题:i.MX280的GPIO电平是1.8V还是3.3V?or 任意GPIO均可单独配置这两种电平? Thanks

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi all,请帮忙解答问题:i.MX280的GPIO电平是1.8V还是3.3V?or 任意GPIO均可单独配置这两种电平? Thanks

ソリューションへジャンプ
1,147件の閲覧回数
alyssawu
Contributor I

Hi all,

请帮忙解答问题:i.MX280的GPIO电平是1.8V还是3.3V?or 任意GPIO均可单独配置这两种电平?

Thanks

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
998件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Q: Please help answer questions: i.MX280 the GPIO level is 1.8V or 3.3V? GPIO can be configured

individually or in any of these two levels? [translated by Google]

Hi alyssa

please refer to sect.9.2.2.2 Pin Voltage Selection MCIMX28RM  :

Each GPIO (non-EMI) pin can be programmed to operate at either 1.8 V or 3.3 V by setting

the bit corresponding to that pin in one of the HW_PINCTRL_DRIVEx registers. The EMI

pins are capable of running at 1.5/1.8 V depending on the EMI_VDDIO voltage.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

如果这个职位回答你的问题,请点击正确答案按钮。谢谢![由谷歌翻译]

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
998件の閲覧回数
alyssawu
Contributor I

坐等回复啊.............:smileyconfused:

0 件の賞賛
返信
999件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Q: Please help answer questions: i.MX280 the GPIO level is 1.8V or 3.3V? GPIO can be configured

individually or in any of these two levels? [translated by Google]

Hi alyssa

please refer to sect.9.2.2.2 Pin Voltage Selection MCIMX28RM  :

Each GPIO (non-EMI) pin can be programmed to operate at either 1.8 V or 3.3 V by setting

the bit corresponding to that pin in one of the HW_PINCTRL_DRIVEx registers. The EMI

pins are capable of running at 1.5/1.8 V depending on the EMI_VDDIO voltage.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

如果这个职位回答你的问题,请点击正确答案按钮。谢谢![由谷歌翻译]

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
998件の閲覧回数
alyssawu
Contributor I

Hi igro,

Thanks for your reply.

Are you the freescale Employee?:smileywink:

0 件の賞賛
返信