HELP!关于rtl8189es在JB4.2.2上的porting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HELP!关于rtl8189es在JB4.2.2上的porting

4,179 Views
jiangshao
Contributor V

尊敬的FAE

 

我有一块客户根据NXPFreescale)的sabresd_mx6dq设计的开发板,使用的是SDIO接口的

Rtl8189esOSAndroid4.2.2. porting过程中遇到了一些问题,急需您的帮助!

 

驱动:RTL8188EUS_RTL8189ES_linux_v4.1.8_9499.20131104.zip

参考文档:android_ref_codes_JB_4.2/Realtek_Wi-Fi_SDK_for_Android_JB_4_2.pdf

 

移植过程基本完全参照Realtek_Wi-Fi_SDK_for_Android_JB_4_2.pdf

 

  • external/wpa_supplicant_8用驱动提供的2_rtw_r8680.20130821.tar.gz替代
  • hardware下对应文件也用驱动提供的2_20130208.tar.gz替代
  • kernel_imx/drivers/net/wireless/rtl8189es下放置1.8_9499.20131104.tar.gz解压后的内容
  • 根据文档修改rc BoardConfig.mk等文件,修改kernel_imx/drivers/net/wireless/下的KconfigMakefile
  • 内核配置中选择编译8189es为模块
  • 手动将h的内容覆盖到kernel_imx/drivers/net/wireless/rtl8189es/include/autoconf.h

 

编译安卓后烧写固件到开发板中。

在安卓的设置-Wi-Fi-》移动滑块

现象:滑块变为打开,右侧显示正在打开Wi-Fi…,大约几秒后,滑块重新变为关闭

如果用logcat监视,可见如下信息:

 

D/WifiService( 2503): setWifiEnabled: true pid=2766, uid=1000

D/BluetoothAdapter( 2766): 1089157384: getState() :  mService = null. Returning STATE_OFF

D/WifiHW  ( 2503): check_wifi_ifname_from_proc: find lo

D/WifiHW  ( 2503): check_wifi_ifname_from_proc: find eth0

D/WifiHW  ( 2503): check_wifi_ifname_from_proc: find tunl0

D/WifiHW  ( 2503): check_wifi_ifname_from_proc: find sit0

D/WifiHW  ( 2503): check_wifi_ifname_from_proc: find ip6tnl0

: 《重复信息》

D/WifiHW  ( 2503): check_wifi_ifname_from_proc: find lo

D/WifiHW  ( 2503): check_wifi_ifname_from_proc: find eth0

D/WifiHW  ( 2503): check_wifi_ifname_from_proc: find tunl0

D/WifiHW  ( 2503): check_wifi_ifname_from_proc: find sit0

D/WifiHW  ( 2503): check_wifi_ifname_from_proc: find ip6tnl0

E/WifiHW  ( 2503): load_driver: get wifi_ifname(PRIMARY) fail

E/WifiStateMachine( 2503): Failed to load driver!

E/WifiStateMachine( 2503): DriverFailedState

D/BluetoothAdapter( 2766): 1089157384: getState() :  mService = null. Returning STATE_OFF

 

 

串口控制台有如下输出:

RTL871X: module init start version:v4.1.8_9499.20131104

RTL871X: rtl8189es driver version=v4.1.8_9499.20131104

RTL871X: build time: Oct 27 2016 13:15:52

RTL871X: module init ret=0

RTL871X: module exit start

RTL871X: module exit success

 

从现象来看,在试图打开wifi时,module先被init,且顺利完成(?)

但是因为找不到wlan0p2p0,导致load_driver: get wifi_ifname(PRIMARY) fail(?)

最终module exit start

 

这大概是哪里的问题呢?

 

我曾经试图让printk输出更多信息,但是

cat proc/sys/kernel/printk

输出为

15    4    1    7

这个15很让人费解,但是似乎已经是输出所有信息了。。。

 

Labels (4)
0 Kudos
Reply
11 Replies

3,135 Views
jiangshao
Contributor V

最近又测试了一个更新版本的驱动,错误依旧。

所以现在有些怀疑是不是:

1,硬件连接问题:在和wifi模块厂家确认

2,板文件设置问题?

目前8189es接在了SD2,板文件中定义如下:

static const struct esdhc_platform_data mx6q_sabresd_sd2_data __initconst = {
.cd_gpio = SABRESD_SD2_CD,
.wp_gpio = SABRESD_SD2_WP,
.keep_power_at_suspend = 1,
// change by shao, 2016-09-21, for rtl8189es
//.support_8bit = 1,
.support_8bit = 0,
.delay_line = 0,
.cd_type = ESDHC_CD_CONTROLLER,
.runtime_pm = 1,
};

不知有没有不妥的地方?

0 Kudos
Reply

3,135 Views
jimmychan
NXP TechSupport
NXP TechSupport

wp is not use. you can remove the .wp_gpio = SABRESD_SD2_WP,

0 Kudos
Reply

3,135 Views
jiangshao
Contributor V

非常感谢,我按照您的提示修改如下,

static const struct esdhc_platform_data mx6q_sabresd_sd2_data __initconst = {
//.cd_gpio = SABRESD_SD2_CD,
//.wp_gpio = SABRESD_SD2_WP,
.always_present = 1,
.keep_power_at_suspend = 1,
//change by shao, 2016-09-21, for rtl8189es
//.support_8bit = 1,
.support_8bit = 0,
.delay_line = 0,
//.cd_type = ESDHC_CD_CONTROLLER,
.cd_type = ESDHC_CD_PERMANENT,
//.runtime_pm = 1,
};

错误有了变化,似乎wlan0出现了,但是p2p0还是没有。。。

D/WifiService( 2504): setWifiEnabled: true pid=2797, uid=1000
D/BluetoothAdapter( 2797): 1092990560: getState() : mService = null. Returning STATE_OFF
D/Tethering( 2504): sendTetherStateChangedBroadcast 1, 0, 0
D/Tethering( 2504): InitialState.processMessage what=4
D/Tethering( 2504): sendTetherStateChangedBroadcast 0, 0, 0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find lo
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find eth0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find tunl0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find sit0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find ip6tnl0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find eth1
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find wlan0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find lo
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find eth0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find tunl0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find sit0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find ip6tnl0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find eth1
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find wlan0
D/SoftapController( 2175): Softap fwReload - Ok
D/CommandListener( 2175): Setting iface cfg
D/CommandListener( 2175): Trying to bring down wlan0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find lo
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find eth0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find tunl0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find sit0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find ip6tnl0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find eth1
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find wlan0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find lo
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find eth0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find tunl0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find sit0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find ip6tnl0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find eth1
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find wlan0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find lo
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find eth0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find tunl0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find sit0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find ip6tnl0
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find eth1
D/WifiHW ( 2504): check_wifi_ifname_from_proc: find wlan0
E/WifiHW ( 2504): wifi_start_supplicant get wifi_ifname(SECONDARY) fail
E/WifiStateMachine( 2504): Failed to start supplicant!
W/Netd ( 2175): No subsystem found in netlink event
D/NetlinkEvent( 2175): Unexpected netlink message. type=0x11
D/BluetoothAdapter( 2797): 1092990560: getState() : mService = null. Returning STATE_OFF

0 Kudos
Reply

3,135 Views
jimmychan
NXP TechSupport
NXP TechSupport

This link may useful for you.

(please check the permission in Android)

https://community.nxp.com/message/801650 

0 Kudos
Reply

3,135 Views
jimmychan
NXP TechSupport
NXP TechSupport

maybe the name setting here is not match in your system:

WIFI_DRIVER_MODULE_NAME := "wlan"
WIFI_DRIVER_MODULE_PATH := "/system/lib/modules/wlan.ko"
WIFI_DRIVER_MODULE_ARG := "ifname=wlan0 if2name=p2p0"

please check the BoardConfig.mk

0 Kudos
Reply

3,135 Views
jiangshao
Contributor V

我们的BoardConfig.mk定义如下:

WPA_SUPPLICANT_VERSION := VER_0_8_X
BOARD_WPA_SUPPLICANT_DRIVER := NL80211
CONFIG_DRIVER_WEXT := y
#CONFIG_DRIVER_NL80211 :=true
BOARD_WPA_SUPPLICANT_PRIVATE_LIB := lib_driver_cmd_rtl
BOARD_HOSTAPD_DRIVER := NL80211
BOARD_HOSTAPD_PRIVATE_LIB := lib_driver_cmd_rtl
BOARD_WLAN_DEVICE := rtl8189es

WIFI_DRIVER_MODULE_NAME := "8189es"
WIFI_DRIVER_MODULE_PATH := "/system/lib/modules/8189es.ko"
WIFI_DRIVER_MODULE_ARG := "ifname=wlan0 if2name=p2p0"

且我已将make modules得到的8189es.ko放入/system/lib/modules/

另外,如果我选择把8189不编译成ko,而是编译进内核,

logcat有如下错误:

D/WifiService( 2579): setWifiEnabled: true pid=2873, uid=1000
D/BluetoothAdapter( 2873): 1108199328: getState() : mService = null. Returning STATE_OFF
E/WifiStateMachine( 2579): Failed to load driver!
E/WifiStateMachine( 2579): DriverFailedState
D/BluetoothAdapter( 2873): 1108199328: getState() : mService = null. Returning STATE_OFF

从dmesg的输出来看

<4>RTL871X: module init start
<4>RTL871X: rtl8189es v4.3.18.1_15373.20151005
<4>RTL871X: build time: Nov 7 2016 15:17:23
<4>RTL871X: module init ret=0

驱动的版本都已经被识别,应该是驱动被找到了。。。

0 Kudos
Reply

3,135 Views
jimmychan
NXP TechSupport
NXP TechSupport

I found this may useful for you.

android-imx6-kitkat/platform/hardware/realtek.git at master · rabeeh/android-imx6-kitkat · GitHub 

Basically, this is realtek driver issue. It is better to consult realtek for the driver solution using in Android.

0 Kudos
Reply

3,135 Views
zhanghaijian
Contributor II

Jimmy 你好!

我现在也碰到了找不到wlan0的问题,请问你是怎么解决的!

0 Kudos
Reply

3,134 Views
jiangshao
Contributor V

附件是全部log,请参考

0 Kudos
Reply

3,133 Views
jimmychan
NXP TechSupport
NXP TechSupport

Can you show the full logcat (from the board boot up to this issue occur)?

0 Kudos
Reply

3,133 Views
jiangshao
Contributor V

刚才上传了log,从3098行开始

0 Kudos
Reply