HDMI Tx without DCSS in IMX8MQ

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HDMI Tx without DCSS in IMX8MQ

1,137 次查看
jemish_1990
Contributor IV

We are going to make product based on IMX8MQ (MIMX8MQ6DVAJZAA) processor.  Currently we are doing POC on IMX8MQ processor EVK.

  • Based Technical Reference manual and sample device tree files what I see that we are always using DCSS controller to drive output on HDMI screen. Is there any way we can use HDMI TX directly without using DCSS controller?
  • Basically we want to use MIPI DSI interface for DSI panel and use DCSS controller for different features (scaling, rotation, overlay etc).
  • And use HDMI display as it is.

Is what I describe here is possible in IMX8MQ?

Thanks,

Jemish

标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

917 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, the DCSS is crucial for the HDMI output on the i.MX8MQ. You cannot have the HDMI output without the use of the DCSS. I apologize for the inconveniences this could give you.

Best regards,

Diego.

0 项奖励
回复

917 次查看
jemish_1990
Contributor IV

Thanks Diego !

It is clear now.

You can mark this discussion as close.

0 项奖励
回复