Hi all,
I've been following this thread gstreamer: video fails to play when opened for second time but as I'm not sure if my problem is the same I'm opening a new one.
My problem is in a iMX28 custom board, and the code I'm running in my application is really trivial:
gst_init (NULL, NULL); |
/* Build the pipeline */
pipeline = gst_parse_launch ("playbin2 uri=file:///mnt/gonzalo/Copreci-heart_x264_200x120_12000_15fps_320_22050.mp4", NULL);
/* Start playing */
gst_element_set_state (pipeline, GST_STATE_PLAYING);
/* Wait until error or EOS */
bus = gst_element_get_bus (pipeline);
msg = gst_bus_timed_pop_filtered (bus, GST_CLOCK_TIME_NONE, GST_MESSAGE_ERROR | GST_MESSAGE_EOS);
/* Free resources */
if (msg != NULL)
gst_message_unref(msg); |
gst_object_unref(bus);
gst_element_set_state(pipeline, GST_STATE_NULL);
gst_object_unref(pipeline);
gst_deinit();
First time I run this code in my application everything goes fine, the video is played nicely. Here is the log:
Aiur: 3.0.6
Core: MPEG4PARSER_06.04.27 build on Dec 20 2012 16:48:05
mime: video/quicktime; audio/x-m4a; application/x-3gp
file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm9_elinux.so.3.1
Content Info:
URI:
file:///mnt/gonzalo/Copreci-heart_x264_200x120_12000_15fps_320_22050.mp4
Idx File:
/root/.aiur/.mnt.gonzalo.Copreci-heart_x264_200x120_12000_15fps_320_22050.mp4.ai
dx
Seekable : Yes
Size(byte): 18666817
Movie Info:
Seekable : Yes
Live : No
Duration : 0:01:41.000000000
ReadMode : File
Track : 2
Track 00 [video_000000] Enabled
Duration: 0:01:41.000000000
Language: eng
Mime:
video/x-h264, parsed=(boolean)true, width=(int)200, height=(int)120, framerate=(
fraction)15/1, codec_data=(buffer)000000016742c00ddb0d11e59610000003001000000301
e0f142ae0000000168ca8cb2
H264D_ARM9_02.06.01 build on Jul 12 2011 14:01:56.
MFW_GST_H264_DECODER_PLUGIN 3.0.6 build on Feb 5 2014 15:30:55.
Track 01 [audio_000000] Enabled
Duration: 0:01:40.850000000
Language: eng
Mime:
audio/mpeg, mpegversion=(int)1, framed=(boolean)true, channels=(int)2, rate=(int
)22050, bitrate=(int)160013
MFW_GST_V4LSINK_PLUGIN 3.0.6 build on Feb 5 2014 15:30:44.
Beep: 3.0.6
Core: MP3 decoder Wrapper build on Jan 16 2013 16:21:07
mime: audio/mpeg, mpegversion = (int)1
file: /usr/lib/imx-mm/audio-codec/wrap/lib_mp3d_wrap_arm9_elinux.so
CODEC: BLN_MAD-MMCODECS_MP3D_ARM_02.13.00_ARM9 build on Dec 5 2012 09:44:32.
>>V4L_SINK: Actually buffer status:
hardware buffer : 21
software buffer : 0
full screen size:480x272
[V4L Update Display]: left=0, top=0, width=480, height=272
Running time 0:01:40.940589569 render fps 14.157
Total rendered:1429
[--->FINALIZE aiurdemux
Second time my application runs the same code I get the following error:
(<unknown>:4591): GStreamer-CRITICAL **: gst_element_set_state: assertion `GST_IS_ELEMENT (element)' failed
(<unknown>:4591): GStreamer-CRITICAL **: gst_element_get_bus: assertion `GST_IS_ELEMENT (element)' failed
(<unknown>:4591): GStreamer-CRITICAL **: gst_bus_timed_pop_filtered: assertion `GST_IS_BUS (bus)' failed
(<unknown>:4591): GStreamer-CRITICAL **: gst_object_unref: assertion `object != NULL' failed
(<unknown>:4591): GStreamer-CRITICAL **: gst_element_set_state: assertion `GST_IS_ELEMENT (element)' failed
(<unknown>:4591): GStreamer-CRITICAL **: gst_object_unref: assertion `object != NULL' failed
If I restart my application, the previous code runs fine but once again, only the first time. I've also tried running the same code from a CHILD process. Doing it this way, the code DOESN'T FAIL, so looks something is not de-initializing properly. But in my application I don't want to run it in a child process, and would like to know what's wrong in this code.
Can someone help me?
Thanks in advance,
Gonzalo.
解決済! 解決策の投稿を見る。
Hi Gonzalo,
I have attached the libmfw_gst_v4lsink.so extracted from the MM codec package 3.0.11. Please use this library file to replace the one in your rootfs. After the change, the repeat mode can work for your H.264 test vectors.
Thanks,
Peter
Hi Gonzalo,
I had a similar bug when I was building the Linux kernel (Freescale 2.6.35 on i.mx53) with the CodeSourcery compiler
Alexander
Hi Alexander,
did you find a solution?
Thanks,
Gonzalo
Hi Gonzalo,
Yeah, I just recompiled the kernel with another compiler without recompiling the entire root file system. Problems were with
gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203)
Alexander.
Hi Alexander,
Freescale's L2.6.35_1.1.0_130130_images_MX28 image is built with the following toolchain:
Linux version 2.6.35.3-670-g914558e (r65388@szx32-17) (gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) ) #1 PREEMPT Wed Jan 30 15:03:15 CST 2013
Anyway, I'll try to find a different toolchain (maybe from Yocto) and find out how to use it in Ltib.
Thanks,
Gonzalo.
Bitbake is baking .......
Let's see what happens
Well, just doesn't work.
I bitbaked fsl-image-test:
.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.
Build Configuration:
BB_VERSION = "1.20.0"
BUILD_SYS = "i686-linux"
NATIVELSBSTRING = "Ubuntu-12.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx28evk"
DISTRO = "poky"
DISTRO_VERSION = "1.5.2"
TUNE_FEATURES = "armv5 thumb dsp"
TARGET_FPU = "soft"
meta
meta-yocto = "GONZALO:7c3f509c065960fed9445cd73e350b7c7ddfd521"
meta-oe = "GONZALO:ee173678383683e972c7d4d6f0ef5790bfa50274"
meta-fsl-arm = "GONZALO:5fdb620c09df11e70434092f675c891e0ba84108"
meta-fsl-arm-extra = "GONZALO:375f89b70655be2a17bbde36de6adb4e4a5a6975"
meta-fsl-demos = "GONZALO:5a12677ad000a926d23c444266722a778ea228a7"
.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.
and when trying to play the video I get and error: Illegal Instruction.
.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.
root@imx28evk:/home/user/video#
8kHz_128kbps_131sec.mp4 /video# gplay Kaleidoscope_h264_qvga_387kbps_30fps_mp3_48
playbin2 is employed!
fsl_player_init(): Successfully initialize!
fsl_player_set_media_location(): filename=Kaleidoscope_h264_qvga_387kbps_30fps_mp3_48kHz_128kbps_131sec.mp4
[Stopped ][Vol=01][00:00:00/00:00:00][fps:0]Aiur: 3.0.9
Core: MPEG4PARSER_06.07.00 build on Sep 10 2013 01:42:25
mime: video/quicktime; audio/x-m4a; application/x-3gp
file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm9_elinux.so.3.2
Content Info:
URI:
file:///home/user/video/Kaleidoscope_h264_qvga_387kbps_30fps_mp3_48kHz_128kbps_1
31sec.mp4
Idx File:
/home/root/.aiur/.home.user.video.Kaleidoscope_h264_qvga_387kbps_30fps_mp3_48kHz
_128kbps_131sec.mp4.aidx
Seekable : Yes
Size(byte): 7689783
[Stopped ][Vol=01][00:00:00/00:00:00][fps:0]Illegal instruction
root@imx28evk:/home/user/video#
.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.
If I use the gplay provided by Peter Chan, it also doesn't work:
.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.
_48kHz_128kbps_131sec.mp4 ideo# ./gplay Kaleidoscope_h264_qvga_387kbps_30fps_mp3_
playbin2 is employed!
fsl_player_init(): Successfully initialize!
fsl_player_set_media_location(): filename=Kaleidoscope_h264_qvga_387kbps_30fps_mp3_48kHz_128kbps_131sec.mp4
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
[Stopped ][Vol=00][00:00:00/00:00:00][fps:160744729699921428480]Aiur: 3.0.9
Core: MPEG4PARSER_06.07.00 build on Sep 10 2013 01:42:25
mime: video/quicktime; audio/x-m4a; application/x-3gp
file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm9_elinux.so.3.2
Content Info:
URI:
file:///home/user/video/Kaleidoscope_h264_qvga_387kbps_30fps_mp3_48kHz_128kbps_1
31sec.mp4
Idx File:
/home/root/.aiur/.home.user.video.Kaleidoscope_h264_qvga_387kbps_30fps_mp3_48kHz
_128kbps_131sec.mp4.aidx
Seekable : Yes
Size(byte): 7689783
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
[Stopped ][Vol=00][00:00:00/00:00:00][fps:160744729699921428480] Aborted by signal Interrupt...
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
[Stopped ][Vol=00][00:00:00/00:00:00][fps:160744729699921428480]Wait status change from 2 to 4
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
[Stopped ][Vol=00][00:00:00/00:00:00][fps:160744729699921428480]fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
[Stopped ][Vol=00][00:00:00/00:00:00][fps:160744729699921428480]Wait status change from 2 to 4
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
[Stopped ][Vol=00][00:00:00/00:00:00][fps:160744729699921428480]fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
fsl_player_rotate(): Can not find auto_video_sink
.......................
.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.
Hi Gonzalo,
I use GDB to debug the gplay and dump the backtrace when mfw_gst_v4l2_close() is called to release the PXP. What is your backtrace when the first video plays to an end?
Breakpoint 2, 0x43931cac in mfw_gst_v4l2_close (v4l_info=0x107160)
at mfw_gst_v4l.c:907
907 mfw_gst_v4l.c: No such file or directory.
in mfw_gst_v4l.c
(gdb) backtrace
#0 0x43931cac in mfw_gst_v4l2_close (v4l_info=0x107160) at mfw_gst_v4l.c:907
#1 0x439357b0 in mfw_gst_v4lsink_finalize (object=0x107160)
at mfw_gst_v4lsink.c:1734
#2 0x402751d4 in IA__g_object_unref (_object=0x107160) at gobject.c:2991
#3 0x401e2ec8 in gst_message_finalize (message=0x16e280) at gstmessage.c:185
#4 0x401e6f6c in gst_mini_object_unref (mini_object=0x16e280)
at gstminiobject.c:604
#5 0x401c15c0 in gst_bus_source_dispatch (source=0x968b8,
callback=<value optimized out>, user_data=0x15040) at gstbus.c:971
#6 0x404df140 in IA__g_main_context_dispatch (context=0x17a00) at gmain.c:3276
#7 0x404df738 in g_main_context_iterate (context=0x17a00,
block=<value optimized out>, dispatch=1) at gmain.c:3276
#8 0x404df984 in IA__g_main_context_iteration (context=0x17a00, may_block=0)
at gmain.c:3276
#9 0x4002b690 in g_main_loop_thread_fun (data=<value optimized out>)
at mfw_gplay_core.c:1417
#10 0x4050584c in g_thread_create_proxy (data=0x95730) at gthread.c:180
#11 0x40052cd0 in start_thread () from /lib/libpthread.so.0
#12 0x40130418 in clone () from /lib/libc.so.6
Hi Peter,
my gbd skills are quite limited. I've installed gdb on the evk and I'm able to launch gplay on gdb, run the mp4 video, set breakpoints, backtrace... but don't know how to set a break point at mfw_gst_v4l.c:907
Please, could you guide me on this??
Thanks,
Gonzalo.
I just set the breakpoint to the function "mfw_gst_v4l2_close" by GDB command "break mfw_gst_v4l2_close". When the gplay stops at the breakpoint, run "backtrace" command to print the stack trace.
More information about GDB commands can be found at http://www.yolinux.com/TUTORIALS/GDB-Commands.html.
Since there is no "FINALIZE v4l_sink" in your log, I don't expect the gplay will stop at the mfw_gst_v4l2_close() breakpoint in your test.
Thanks a lot, Peter !!
As you were expecting, gplay doesn't stop at mfw_gst_v4l2_close(). Attached you can find the complete log.
The log is from the iMX28-evk running L2.6.35_1.1.0_130130_images_MX28, where I've deleted the original "gplay" and have run the patched "gplay" with the bug you found already fixed.
Previously I tried the original "gplay" with the same results.
Furthermore, I've never seen the "FINALIZE v4l_sink" message, even if a run "gplay" with no repetitions.
Thanks,
Gonzalo.
I have no idea why the "FINALIZE v4l_sink" did not execute even we are using the same prebuilt image. Are you using the MX28 LCD daughter card MCIMX28LCD Seiko 4/3" WVGA Rev B? Can we testing with the same video?
This video is transcoded from https://community.freescale.com/docs/DOC-93383 with the setting {Video codec: MPEG-4 constant framerate & quality, Audio Codec: MP3 (Lame) 128kbps 44100 Hz}. Using this video, "FINALIZE v4l_sink" will execute when it plays to an end in gplay.
Hi Peter,
Yes, I'm using the iMX28-evk with a "MCIMX28LCD Seiko 4/3" WVGA Rev B"
You are right !!! Your video file is playing fine, repeating continously with no problem, and I can see the expected [--->FINALIZE v4l_sink at the end of every repetition.
I'm attaching the complete log for 4 repetitions.
Do you know what could be the problem decoding my video file?
Thanks,
Gonzalo.
My video transcoder is downloaded from HandBrake: Open Source Video Transcoder.
Can you share your video to me so that we can further investigate this issue?
Does this problem all happen to all videos you got? How did you get these videos?
Hi Peter,
you can find the video file I was using in this same thread, in my post on 03-jul-2014 18:04 (Re: Re: Re: Gstreamer not working second time) I don't know the way it was trancoded. I got it from my Freescales's local FAE.
And yes, I've found this problem in all my video files, transcoded using Any Video Converter (Free Video Converter, Any Video Converter Freeware: Convert any video to MP4/WMV/MP3 for mobile devi...)
Thanks,
Gonzalo.
Would you please transcode the video at https://community.freescale.com/docs/DOC-93383 and send me to test?
Yes, I'll do it tomorrow. I'm out of the office and don't have access to a Windows machine.
Thanks,
Gonzalo
Hi Peter,
attached you can find 2 video files I've got transcoding VID_20120917_211055[1].mp4
Both of them don't play smoothly at all on the iMX28evk but when playing
- VID_20120917_211055[1]_x264_KO.mp4: it shows the problem I've reported in this thread.
- VID_20120917_211055[1]_x264_OK.mp4: gplay can repeat it with no problem.
Thanks,
Gonzalo.
Hi again Peter,
I've been doing a lot of testing during this weekend and haven't come to a conclusion but I've got some filling.
The issue looks to be related to how the video is encoded in the mp4 file:
- MPEG-4 encoded video plays quite smoothly, and I think I've always seen the [--->FINALIZE v4l_sink message at the end of every repetition.
- H.264 (x264) encoded video plays more chunky, and it's hard to get a file that shows the [--->FINALIZE v4l_sink message at the end of every repetition.
Does this make any sense for you?
Thanks,
Gonzalo.
I agree with your findings. In your application, is it mandatory to have H.264 support in your application? It looks the H.264 decode is more CPU demanding for the same video quality.
Unfortunately, yes, h.264 is required.