Gstreamer library not working on imx8mm evk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Gstreamer library not working on imx8mm evk

1,271件の閲覧回数
TBYE
Contributor I

I am using imx8m evk with imx-image-core, in which while fetching feed from camera getting internal stream error from gstreamer.

Attached are the result gst-device-monitor and gst-inpect-1.0.gst-device-monitor.JPGgst-inspect-1.0-output.JPG

0 件の賞賛
返信
5 返答(返信)

1,225件の閲覧回数
TBYE
Contributor I

Erza_0-1615980446045.png

Adding packagegroup-fsl-gstreamer1.0 in imx-image-core.bb file resolves the gstreamer issue.

0 件の賞賛
返信

1,249件の閲覧回数
TBYE
Contributor I

I am using imx-image-core , kernel 5.4.24 built using instruction provided by imx- yocto guide. It is working fine with imx-image-full.

Erza_0-1615264965849.png

 

0 件の賞賛
返信

1,241件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

1,255件の閲覧回数
TBYE
Contributor I

 

 

0 件の賞賛
返信

1,263件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Erza

 

what bsp used in the case, one can try Demo Image  i.MX 8M Mini EVK

use Chapter 7 Multimedia   i.MX Linux User’s Guide​

 

Best regards
igor

0 件の賞賛
返信