GPS MODULE AND 3g MODULE FOR I.MX 53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPS MODULE AND 3g MODULE FOR I.MX 53

1,155 Views
farzinfarzini
Contributor II

Hi Friend
Gps module with a compatible bsp for tablet i.mx535.
Apart from the gm22 AR1520A
You know?

I can not find the gm22 on mouser and findchipd.com?

Part numbers for the 3g module on tablets sabre you know?

If possible, you give numbers?

Alternative models You know?

For wifi / bt is also athors Part Number to buy it You know?


  huawei 820 u to do this right?

Labels (5)
3 Replies

955 Views
igorpadykov
NXP Employee
NXP Employee

Hi FRARZIN

supported chips are described in Linux Manual

(mx53_sabre_tablet_linux.pdf) included in

IMX53_1109_LINUXDOCS_BUNDLE

and i.MX_Android_R10.x_Release_Note.html included in

IMX5X_R10_31_ANDROID_DOCSBUNDLE

such as 3g HuaWei EM750M/E180/E220/E770M (HSPA/WCDMA/GPRS).

For new modules (not mentioned in these documents) you will have to add

support (driver for new module).

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

955 Views
farzinfarzini
Contributor II

TANKS for answer

for Gps module with a compatible bsp for tablet i.mx535.

Apart from the gm22 AR1520A

You know?

0 Kudos
Reply

955 Views
igorpadykov
NXP Employee
NXP Employee

Hi FRARZIN

BSP is written for specific chips, which

are used on Freescale reference boards.

For other chips one needs to add driver for them.

Best regards

chip

0 Kudos
Reply