I am a beginner and i am trying to install multimedia packages on L3.0.35_4.1.0 for my iMX6 custom board which has SGTL5000 on it.
The Freescale Multimedia Users guide says while building codec packages in LTIB,
Copy these standard packages to the LPP directory, which, by default, is set to /var/
tmp/pkgs (see litb/.ltibrc %ldirs).
If you are installing LTIB for the first time, you need to
create this directory manually.
I have obtained all the packages from https://community.freescale.com/docs/DOC-95560
and i am building LTIB for the first time. But i am not able to figure out the location where i have to create a LPP directory and place the codecs manually in it.
And what should be the name of the directory.
I would appreciate an explanatory answer of the entire process.
thanks,
nishad
Solved! Go to Solution.
Hi nishad,
You can make a directory pkgs under /var/tmp, and copy the packages you have download to /var/tmp/pkgs. Then you can go next step to build them. More details you can refer to the document i.MX_6_Ubuntu_Multimedia_User_Guide.pdf. Hope this can help you.
Have a great day
Best Regards
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi nishad,
You can make a directory pkgs under /var/tmp, and copy the packages you have download to /var/tmp/pkgs. Then you can go next step to build them. More details you can refer to the document i.MX_6_Ubuntu_Multimedia_User_Guide.pdf. Hope this can help you.
Have a great day
Best Regards
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------